- Mon Apr 11, 2022 9:41 am
#232507
Hi every body,
I just start to use both modules and I see that the data rate is permanently around 10 Hz even if configured for 25Hz and even with a clear sky.
As the NEO is announced to work up to 25 Hz, I am looking for the procedure to increase the rate.
I have also noted that the rate becomes announced 25Hz when the GPS is disconnected.
Christian
I just start to use both modules and I see that the data rate is permanently around 10 Hz even if configured for 25Hz and even with a clear sky.
As the NEO is announced to work up to 25 Hz, I am looking for the procedure to increase the rate.
I have also noted that the rate becomes announced 25Hz when the GPS is disconnected.
Christian