- Tue May 20, 2008 8:48 pm
#48687
(OLED, fresh after a reset)
Hi all,
I thought I might move some discussion for this topic about finding some 2.8" OLED displays to the project forum, since I'm actually working on figuring out how to interface with one of them!
viewtopic.php?t=9843
a quick summary: The display is a 2.8" OLED display from OSD displays, which are (I think) the same as the ones from vision-opto, and the ones used on the 4D systems OLED displays. The display uses a S6E63D6 controller that has both parallel and SPI interfaces. I have been trying to write pixel data to the display using the SPI interface. The display's datasheet can be found here:
S6E63D6 Controller:
http://www.cec-mc.ru/comp/lcd/powertip/pdf/S6E63D6.pdf
A sample pinout from vision-opto: (I'm not sure I can post the OSD datasheet?)
http://vision-opto.com/C0283QGLF-T%202. ... 20SPEC.pdf
platform: my friend, the dsPIC33FJ356MC710 over SPI.
general spi interface information: reads/writes are generally 3-bytes. The first byte is a start byte, followed by two data bytes. The start byte contains an ID, plus a 'read/write' and 'address or data' flag. to actually read or write data to an address you'd have to send two packets of information: one to set the address, and the next to read/write to/from that address.
most of the addresses are internal registers that let you setup the display parameters, like size, colour depth, etc.
writing pixel data (to 'GRAM') is a little different: first you have to set the x,y coordinates by writing data to addresses 20 (x) and 21 (y), then write the actual pixel data (RGB) to address 22.
---
progress:
write instruction address: ok
read instruction address: not supported by display (returns the current line the display is updating)
write data to address: ok
read data from address: ok
problems:
1: i seem to be able to write data to and from the display registers okay, EXCEPT that the GRAM access doesn't appear to be functioning properly. I'll write the x,y coordinates to 20h/21h, and some data to 22h. When I read back 20/21h, they contain the original address I set it to, but 22h generally contains wierd (random?) data. 20h/21h are supposed to automatically increment after a write to 22h.
2: the display appears to power OK, and powers to a pure white state. setting register 10h to 0000h takes the display out of stand-by, and the display turns to pure black. setting register 05h to 0001h is supposed to start displaying the frame data (in the GRAM) to the display. when i do this, the display turns mostly white with some grey streaky lines horizontally across it. (note: pictures below)
3: writes to GRAM don't appear to work while the display is in stand-by, out of stand-by (10h), displaying the frame, or not displaying the frame (05h).
4: from a restart, (pulling the displays restart pin temporarily low), if I set 05h to 0001h, it will stay at 0001. If I then set 10h to 0000h, 05h will turn to 0003h. If I set 10h:0000h then 05h:0001h, 05h will also be 0003h the next time i read it.
5: i've dumped the contents of the registers (00:FFh) (pasted below), and the contents of some of them right after a reset appear different then the default values reported in the datasheet.
summary:
- reads/writes to registers appear okay, but not to GRAM.
- wierd streaky data is displayed when DISP_ON is set to 1 (05h), but nothing I write.
- I'm lost as to why this isn't working.... I have 3.3v into the dsPIC and the display ('Analog voltage' : Pins 3, 54, and IOVCC (VDD3 in S6E63D3 datasheet?): Pin 20), and about +/-4.5/5.0v for the positive/negitive OLED voltages. I've tested the '1st/2nd booster output voltages' right before the cap, and they appear to be 1st: ~2.7-3.0v (oscillates very quickly), and 2nd: ~3v? (i think -- and this one should be negative!) -- but if it's an issue with voltages, I'm not sure why everything on the controller would work but the GRAM, or why the booster voltage would be off in the first place....
OLED: (1) after reset, (2) standby off (10h:0000h)
OLED: (1) after reset, (2) standby off (10h:0000h), (3) DISP_ON (05h:0001h). (The display is white with some grey horizontal streaks. Sorry the picture is so bloomed!)
register dump after reset: (sorry the indicies aren't in hex!)
(OLED, fresh after a reset)
Hi all,
I thought I might move some discussion for this topic about finding some 2.8" OLED displays to the project forum, since I'm actually working on figuring out how to interface with one of them!
viewtopic.php?t=9843
a quick summary: The display is a 2.8" OLED display from OSD displays, which are (I think) the same as the ones from vision-opto, and the ones used on the 4D systems OLED displays. The display uses a S6E63D6 controller that has both parallel and SPI interfaces. I have been trying to write pixel data to the display using the SPI interface. The display's datasheet can be found here:
S6E63D6 Controller:
http://www.cec-mc.ru/comp/lcd/powertip/pdf/S6E63D6.pdf
A sample pinout from vision-opto: (I'm not sure I can post the OSD datasheet?)
http://vision-opto.com/C0283QGLF-T%202. ... 20SPEC.pdf
platform: my friend, the dsPIC33FJ356MC710 over SPI.
general spi interface information: reads/writes are generally 3-bytes. The first byte is a start byte, followed by two data bytes. The start byte contains an ID, plus a 'read/write' and 'address or data' flag. to actually read or write data to an address you'd have to send two packets of information: one to set the address, and the next to read/write to/from that address.
most of the addresses are internal registers that let you setup the display parameters, like size, colour depth, etc.
writing pixel data (to 'GRAM') is a little different: first you have to set the x,y coordinates by writing data to addresses 20 (x) and 21 (y), then write the actual pixel data (RGB) to address 22.
---
progress:
write instruction address: ok
read instruction address: not supported by display (returns the current line the display is updating)
write data to address: ok
read data from address: ok
problems:
1: i seem to be able to write data to and from the display registers okay, EXCEPT that the GRAM access doesn't appear to be functioning properly. I'll write the x,y coordinates to 20h/21h, and some data to 22h. When I read back 20/21h, they contain the original address I set it to, but 22h generally contains wierd (random?) data. 20h/21h are supposed to automatically increment after a write to 22h.
2: the display appears to power OK, and powers to a pure white state. setting register 10h to 0000h takes the display out of stand-by, and the display turns to pure black. setting register 05h to 0001h is supposed to start displaying the frame data (in the GRAM) to the display. when i do this, the display turns mostly white with some grey streaky lines horizontally across it. (note: pictures below)
3: writes to GRAM don't appear to work while the display is in stand-by, out of stand-by (10h), displaying the frame, or not displaying the frame (05h).
4: from a restart, (pulling the displays restart pin temporarily low), if I set 05h to 0001h, it will stay at 0001. If I then set 10h to 0000h, 05h will turn to 0003h. If I set 10h:0000h then 05h:0001h, 05h will also be 0003h the next time i read it.
5: i've dumped the contents of the registers (00:FFh) (pasted below), and the contents of some of them right after a reset appear different then the default values reported in the datasheet.
summary:
- reads/writes to registers appear okay, but not to GRAM.
- wierd streaky data is displayed when DISP_ON is set to 1 (05h), but nothing I write.
- I'm lost as to why this isn't working.... I have 3.3v into the dsPIC and the display ('Analog voltage' : Pins 3, 54, and IOVCC (VDD3 in S6E63D3 datasheet?): Pin 20), and about +/-4.5/5.0v for the positive/negitive OLED voltages. I've tested the '1st/2nd booster output voltages' right before the cap, and they appear to be 1st: ~2.7-3.0v (oscillates very quickly), and 2nd: ~3v? (i think -- and this one should be negative!) -- but if it's an issue with voltages, I'm not sure why everything on the controller would work but the GRAM, or why the booster voltage would be off in the first place....
OLED: (1) after reset, (2) standby off (10h:0000h)
OLED: (1) after reset, (2) standby off (10h:0000h), (3) DISP_ON (05h:0001h). (The display is white with some grey horizontal streaks. Sorry the picture is so bloomed!)
register dump after reset: (sorry the indicies aren't in hex!)
Code: Select all
Update Address Symbol Name Value Hex Binary Decimal
2BA0 reg_data
2BA0 [0] 0x0000 0x0000 00000000 00000000 0
2BA2 [1] 0x8828 0x8828 10001000 00101000 34856
2BA4 [2] 0x0000 0x0000 00000000 00000000 0
2BA6 [3] 0x8030 0x8030 10000000 00110000 32816
2BA8 [4] 0x0000 0x0000 00000000 00000000 0
2BAA [5] 0x0000 0x0000 00000000 00000000 0
2BAC [6] 0x0000 0x0000 00000000 00000000 0
2BAE [7] 0x1200 0x1200 00010010 00000000 4608
2BB0 [8] 0x1212 0x1212 00010010 00010010 4626
2BB2 [9] 0x8422 0x8422 10000100 00100010 33826
2BB4 [10] 0x0000 0x0000 00000000 00000000 0
2BB6 [11] 0x0000 0x0000 00000000 00000000 0
2BB8 [12] 0x0000 0x0000 00000000 00000000 0
2BBA [13] 0x0000 0x0000 00000000 00000000 0
2BBC [14] 0x0000 0x0000 00000000 00000000 0
2BBE [15] 0x63D6 0x63D6 01100011 11010110 25558
2BC0 [16] 0x01C7 0x01C7 00000001 11000111 455
2BC2 [17] 0x0000 0x0000 00000000 00000000 0
2BC4 [18] 0x0008 0x0008 00000000 00001000 8
2BC6 [19] 0x146A 0x146A 00010100 01101010 5226
2BC8 [20] 0x4202 0x4202 01000010 00000010 16898
2BCA [21] 0x0000 0x0000 00000000 00000000 0
2BCC [22] 0x0000 0x0000 00000000 00000000 0
2BCE [23] 0x0000 0x0000 00000000 00000000 0
2BD0 [24] 0x001F 0x001F 00000000 00011111 31
2BD2 [25] 0x0000 0x0000 00000000 00000000 0
2BD4 [26] 0x0005 0x0005 00000000 00000101 5
2BD6 [27] 0x0000 0x0000 00000000 00000000 0
2BD8 [28] 0x0000 0x0000 00000000 00000000 0
2BDA [29] 0x0000 0x0000 00000000 00000000 0
2BDC [30] 0x0000 0x0000 00000000 00000000 0
2BDE [31] 0x0000 0x0000 00000000 00000000 0
2BE0 [32] 0x0000 0x0000 00000000 00000000 0
2BE2 [33] 0x0000 0x0000 00000000 00000000 0
2BE4 [34] 0xA000 0xA000 10100000 00000000 40960
2BE6 [35] 0x0000 0x0000 00000000 00000000 0
2BE8 [36] 0x0000 0x0000 00000000 00000000 0
2BEA [37] 0x0000 0x0000 00000000 00000000 0
2BEC [38] 0x0000 0x0000 00000000 00000000 0
2BEE [39] 0x0000 0x0000 00000000 00000000 0
2BF0 [40] 0x0000 0x0000 00000000 00000000 0
2BF2 [41] 0x0000 0x0000 00000000 00000000 0
2BF4 [42] 0x0000 0x0000 00000000 00000000 0
2BF6 [43] 0x0000 0x0000 00000000 00000000 0
2BF8 [44] 0x0000 0x0000 00000000 00000000 0
2BFA [45] 0x0000 0x0000 00000000 00000000 0
2BFC [46] 0x0000 0x0000 00000000 00000000 0
2BFE [47] 0x0000 0x0000 00000000 00000000 0
2C00 [48] 0x0000 0x0000 00000000 00000000 0
2C02 [49] 0x013F 0x013F 00000001 00111111 319
2C04 [50] 0x0000 0x0000 00000000 00000000 0
2C06 [51] 0x0000 0x0000 00000000 00000000 0
2C08 [52] 0x013F 0x013F 00000001 00111111 319
2C0A [53] 0x0000 0x0000 00000000 00000000 0
2C0C [54] 0x013F 0x013F 00000001 00111111 319
2C0E [55] 0x00EF 0x00EF 00000000 11101111 239
2C10 [56] 0x0000 0x0000 00000000 00000000 0
2C12 [57] 0x0000 0x0000 00000000 00000000 0
2C14 [58] 0x007A 0x007A 00000000 01111010 122
2C16 [59] 0x0022 0x0022 00000000 00100010 34
2C18 [60] 0x0000 0x0000 00000000 00000000 0
2C1A [61] 0x0000 0x0000 00000000 00000000 0
2C1C [62] 0x0000 0x0000 00000000 00000000 0
2C1E [63] 0x0000 0x0000 00000000 00000000 0
2C20 [64] 0x0000 0x0000 00000000 00000000 0
2C22 [65] 0x0010 0x0010 00000000 00010000 16
2C24 [66] 0x0000 0x0000 00000000 00000000 0
2C26 [67] 0x0333 0x0333 00000011 00110011 819
2C28 [68] 0x4281 0x4281 01000010 10000001 17025
2C2A [69] 0x0000 0x0000 00000000 00000000 0
2C2C [70] 0x1122 0x1122 00010001 00100010 4386
2C2E [71] 0x1222 0x1222 00010010 00100010 4642
2C30 [72] 0x0A37 0x0A37 00001010 00110111 2615
2C32 [73] 0x0009 0x0009 00000000 00001001 9
2C34 [74] 0x01AD 0x01AD 00000001 10101101 429
2C36 [75] 0x0000 0x0000 00000000 00000000 0
2C38 [76] 0x0000 0x0000 00000000 00000000 0
2C3A [77] 0x0000 0x0000 00000000 00000000 0
2C3C [78] 0x0000 0x0000 00000000 00000000 0
2C3E [79] 0x0000 0x0000 00000000 00000000 0
2C40 [80] 0x0001 0x0001 00000000 00000001 1
2C42 [81] 0x0000 0x0000 00000000 00000000 0
2C44 [82] 0x0000 0x0000 00000000 00000000 0
2C46 [83] 0x0000 0x0000 00000000 00000000 0
2C48 [84] 0x0000 0x0000 00000000 00000000 0
2C4A [85] 0x0000 0x0000 00000000 00000000 0
2C4C [86] 0x0000 0x0000 00000000 00000000 0
2C4E [87] 0x0000 0x0000 00000000 00000000 0
2C50 [88] 0x0000 0x0000 00000000 00000000 0
2C52 [89] 0x0000 0x0000 00000000 00000000 0
2C54 [90] 0x0000 0x0000 00000000 00000000 0
2C56 [91] 0x0000 0x0000 00000000 00000000 0
2C58 [92] 0x0000 0x0000 00000000 00000000 0
2C5A [93] 0x0000 0x0000 00000000 00000000 0
2C5C [94] 0x0000 0x0000 00000000 00000000 0
2C5E [95] 0x0000 0x0000 00000000 00000000 0
2C60 [96] 0x00F0 0x00F0 00000000 11110000 240
2C62 [97] 0x0111 0x0111 00000001 00010001 273
2C64 [98] 0x0000 0x0000 00000000 00000000 0
2C66 [99] 0x0000 0x0000 00000000 00000000 0
2C68 [100] 0x0000 0x0000 00000000 00000000 0
2C6A [101] 0x0000 0x0000 00000000 00000000 0
2C6C [102] 0x0000 0x0000 00000000 00000000 0
2C6E [103] 0x0000 0x0000 00000000 00000000 0
2C70 [104] 0x0000 0x0000 00000000 00000000 0
2C72 [105] 0x0000 0x0000 00000000 00000000 0
2C74 [106] 0x0000 0x0000 00000000 00000000 0
2C76 [107] 0x0000 0x0000 00000000 00000000 0
2C78 [108] 0x0000 0x0000 00000000 00000000 0
2C7A [109] 0x0000 0x0000 00000000 00000000 0
2C7C [110] 0x0000 0x0000 00000000 00000000 0
2C7E [111] 0x0000 0x0000 00000000 00000000 0
2C80 [112] 0x2580 0x2580 00100101 10000000 9600
2C82 [113] 0x2780 0x2780 00100111 10000000 10112
2C84 [114] 0x3380 0x3380 00110011 10000000 13184
2C86 [115] 0x1D18 0x1D18 00011101 00011000 7448
2C88 [116] 0x1F11 0x1F11 00011111 00010001 7953
2C8A [117] 0x2419 0x2419 00100100 00011001 9241
2C8C [118] 0x1A14 0x1A14 00011010 00010100 6676
2C8E [119] 0x211A 0x211A 00100001 00011010 8474
2C90 [120] 0x2013 0x2013 00100000 00010011 8211
2C92 [121] 0x0000 0x0000 00000000 00000000 0
2C94 [122] 0x0000 0x0000 00000000 00000000 0
2C96 [123] 0x0000 0x0000 00000000 00000000 0
2C98 [124] 0x0000 0x0000 00000000 00000000 0
2C9A [125] 0x0000 0x0000 00000000 00000000 0
2C9C [126] 0x0000 0x0000 00000000 00000000 0
2C9E [127] 0x0000 0x0000 00000000 00000000 0
2CA0 [128] 0x0000 0x0000 00000000 00000000 0
2CA2 [129] 0x0000 0x0000 00000000 00000000 0
2CA4 [130] 0x0000 0x0000 00000000 00000000 0
2CA6 [131] 0x0000 0x0000 00000000 00000000 0
2CA8 [132] 0x0000 0x0000 00000000 00000000 0
2CAA [133] 0x0000 0x0000 00000000 00000000 0
2CAC [134] 0x0000 0x0000 00000000 00000000 0
2CAE [135] 0x0000 0x0000 00000000 00000000 0
2CB0 [136] 0x0000 0x0000 00000000 00000000 0
2CB2 [137] 0x0000 0x0000 00000000 00000000 0
2CB4 [138] 0x0000 0x0000 00000000 00000000 0
2CB6 [139] 0x0000 0x0000 00000000 00000000 0
2CB8 [140] 0x0000 0x0000 00000000 00000000 0
2CBA [141] 0x0000 0x0000 00000000 00000000 0
2CBC [142] 0x0000 0x0000 00000000 00000000 0
2CBE [143] 0x0000 0x0000 00000000 00000000 0
2CC0 [144] 0x0000 0x0000 00000000 00000000 0
2CC2 [145] 0x0000 0x0000 00000000 00000000 0
2CC4 [146] 0x0000 0x0000 00000000 00000000 0
2CC6 [147] 0x0000 0x0000 00000000 00000000 0
2CC8 [148] 0x0000 0x0000 00000000 00000000 0
2CCA [149] 0x0000 0x0000 00000000 00000000 0
2CCC [150] 0x0000 0x0000 00000000 00000000 0
2CCE [151] 0x0000 0x0000 00000000 00000000 0
2CD0 [152] 0x0000 0x0000 00000000 00000000 0
2CD2 [153] 0x0000 0x0000 00000000 00000000 0
2CD4 [154] 0x0000 0x0000 00000000 00000000 0
2CD6 [155] 0x0000 0x0000 00000000 00000000 0
2CD8 [156] 0x0000 0x0000 00000000 00000000 0
2CDA [157] 0x0000 0x0000 00000000 00000000 0
2CDC [158] 0x0000 0x0000 00000000 00000000 0
2CDE [159] 0x0000 0x0000 00000000 00000000 0
2CE0 [160] 0x0000 0x0000 00000000 00000000 0
2CE2 [161] 0x0000 0x0000 00000000 00000000 0
2CE4 [162] 0x0000 0x0000 00000000 00000000 0
2CE6 [163] 0x0000 0x0000 00000000 00000000 0
2CE8 [164] 0x0000 0x0000 00000000 00000000 0
2CEA [165] 0x0000 0x0000 00000000 00000000 0
2CEC [166] 0x0000 0x0000 00000000 00000000 0
2CEE [167] 0x0000 0x0000 00000000 00000000 0
2CF0 [168] 0x0000 0x0000 00000000 00000000 0
2CF2 [169] 0x0000 0x0000 00000000 00000000 0
2CF4 [170] 0x0000 0x0000 00000000 00000000 0
2CF6 [171] 0x0000 0x0000 00000000 00000000 0
2CF8 [172] 0x0000 0x0000 00000000 00000000 0
2CFA [173] 0x0000 0x0000 00000000 00000000 0
2CFC [174] 0x0000 0x0000 00000000 00000000 0
2CFE [175] 0x0000 0x0000 00000000 00000000 0
2D00 [176] 0x0000 0x0000 00000000 00000000 0
2D02 [177] 0x0000 0x0000 00000000 00000000 0
2D04 [178] 0x0000 0x0000 00000000 00000000 0
2D06 [179] 0x0000 0x0000 00000000 00000000 0
2D08 [180] 0x0000 0x0000 00000000 00000000 0
2D0A [181] 0x0000 0x0000 00000000 00000000 0
2D0C [182] 0x0000 0x0000 00000000 00000000 0
2D0E [183] 0x0000 0x0000 00000000 00000000 0
2D10 [184] 0x0000 0x0000 00000000 00000000 0
2D12 [185] 0x0000 0x0000 00000000 00000000 0
2D14 [186] 0x0000 0x0000 00000000 00000000 0
2D16 [187] 0x0000 0x0000 00000000 00000000 0
2D18 [188] 0x0000 0x0000 00000000 00000000 0
2D1A [189] 0x0000 0x0000 00000000 00000000 0
2D1C [190] 0x0000 0x0000 00000000 00000000 0
2D1E [191] 0x0000 0x0000 00000000 00000000 0
2D20 [192] 0x0000 0x0000 00000000 00000000 0
2D22 [193] 0x0000 0x0000 00000000 00000000 0
2D24 [194] 0x0000 0x0000 00000000 00000000 0
2D26 [195] 0x0000 0x0000 00000000 00000000 0
2D28 [196] 0x0000 0x0000 00000000 00000000 0
2D2A [197] 0x0000 0x0000 00000000 00000000 0
2D2C [198] 0x0000 0x0000 00000000 00000000 0
2D2E [199] 0x0000 0x0000 00000000 00000000 0
2D30 [200] 0x0000 0x0000 00000000 00000000 0
2D32 [201] 0x0000 0x0000 00000000 00000000 0
2D34 [202] 0x0000 0x0000 00000000 00000000 0
2D36 [203] 0x0000 0x0000 00000000 00000000 0
2D38 [204] 0x0000 0x0000 00000000 00000000 0
2D3A [205] 0x0000 0x0000 00000000 00000000 0
2D3C [206] 0x0000 0x0000 00000000 00000000 0
2D3E [207] 0x0000 0x0000 00000000 00000000 0
2D40 [208] 0x0000 0x0000 00000000 00000000 0
2D42 [209] 0x0000 0x0000 00000000 00000000 0
2D44 [210] 0x0000 0x0000 00000000 00000000 0
2D46 [211] 0x0000 0x0000 00000000 00000000 0
2D48 [212] 0x0000 0x0000 00000000 00000000 0
2D4A [213] 0x0000 0x0000 00000000 00000000 0
2D4C [214] 0x0000 0x0000 00000000 00000000 0
2D4E [215] 0x0000 0x0000 00000000 00000000 0
2D50 [216] 0x0000 0x0000 00000000 00000000 0
2D52 [217] 0x0000 0x0000 00000000 00000000 0
2D54 [218] 0x0000 0x0000 00000000 00000000 0
2D56 [219] 0x0000 0x0000 00000000 00000000 0
2D58 [220] 0x0000 0x0000 00000000 00000000 0
2D5A [221] 0x0000 0x0000 00000000 00000000 0
2D5C [222] 0x0000 0x0000 00000000 00000000 0
2D5E [223] 0x0000 0x0000 00000000 00000000 0
2D60 [224] 0x0000 0x0000 00000000 00000000 0
2D62 [225] 0x0000 0x0000 00000000 00000000 0
2D64 [226] 0x0000 0x0000 00000000 00000000 0
2D66 [227] 0x0000 0x0000 00000000 00000000 0
2D68 [228] 0x0000 0x0000 00000000 00000000 0
2D6A [229] 0x0000 0x0000 00000000 00000000 0
2D6C [230] 0x0000 0x0000 00000000 00000000 0
2D6E [231] 0x0000 0x0000 00000000 00000000 0
2D70 [232] 0x0000 0x0000 00000000 00000000 0
2D72 [233] 0x0000 0x0000 00000000 00000000 0
2D74 [234] 0x0000 0x0000 00000000 00000000 0
2D76 [235] 0x0000 0x0000 00000000 00000000 0
2D78 [236] 0x0000 0x0000 00000000 00000000 0
2D7A [237] 0x0000 0x0000 00000000 00000000 0
2D7C [238] 0x0000 0x0000 00000000 00000000 0
2D7E [239] 0x0000 0x0000 00000000 00000000 0
2D80 [240] 0x0000 0x0000 00000000 00000000 0
2D82 [241] 0x0006 0x0006 00000000 00000110 6
2D84 [242] 0x0000 0x0000 00000000 00000000 0
2D86 [243] 0x0000 0x0000 00000000 00000000 0
2D88 [244] 0x0023 0x0023 00000000 00100011 35
2D8A [245] 0x6D95 0x6D95 01101101 10010101 28053
2D8C [246] 0x006D 0x006D 00000000 01101101 109
2D8E [247] 0x000C 0x000C 00000000 00001100 12
2D90 [248] 0x0014 0x0014 00000000 00010100 20
2D92 [249] 0x0014 0x0014 00000000 00010100 20
2D94 [250] 0x0030 0x0030 00000000 00110000 48
2D96 [251] 0x0001 0x0001 00000000 00000001 1
2D98 [252] 0x001C 0x001C 00000000 00011100 28
2D9A [253] 0x03FF 0x03FF 00000011 11111111 1023
2D9C [254] 0x00B3 0x00B3 00000000 10110011 179
2D9E [255] 0x0002 0x0002 00000000 00000010 2