- Mon Oct 12, 2009 5:11 pm
#82887
As promised, please find a fully GPL compliant binary version of OpenOCD (v0.3.0-dev 2009.10.12) for Windows 64 bit systems.
DOWNLOAD HERE
README:
I will post the compilation steps later on.
Enjoy!
DOWNLOAD HERE
README:
Code: Select all
Note that since it is still a bit experimental, it was compiled with debug information, so that you can use WPG System64's gdb in case of problemsThis is a development version of OpenOCD 0.3.0 for Windows 64 bit systems (Vista x64, Windows 7 x64)
This version was compiled with WPG System64 (MinGW x64) using the 2009.10.12 version of the OpenOCD
GIT tree and is fully GPL compliant through the use of libftdi/libusb.
To run OpenOCD on Windows 64 bit, you must first install the 64 bit LibUSB drivers by following the
instructions in .\driver\INSTALL.txt
This version of OpenOCD was successfully tested on Vista x64 with an FT2232 based SheevaPlug Dev Kit.
The drivers provided with this release should support the following hardware:
- Amontec JTAGkey
- CALAO Systems USB-A9260
- egnite Turtelizer 2
- Hitex Cortino
- Hitex STM32-PerformanceStick
- Hitex STR9-comStick
- Hubert Hoegl's USB to JTAG
- Joern Kaipf's OOCDLink
- Luminary Micro BD-ICDI In-Circuit Debug Interface Board
- Luminary Micro Stellaris LM3S811 Evaluation Kit
- Marvell SheevaPlug Development Kit
- Olimex ARM-USB-OCD
- Olimex ARM-USB-TINY
- Section5 ICEBear
- Section5 ICEBear
- TinCanTools Flyswatter
- Xverve Signalyzer
I will post the compilation steps later on.
Enjoy!