- Fri May 02, 2008 9:23 pm
#47535
I bought the Motion Detection Module - MSP430F2013 http://www.sparkfun.com/commerce/produc ... ts_id=8645 from spark fun and it works when power from coin cell or JTAG. However, I am unable to program the micro controller using mspgcc. Keep in mind that I have successfully programed Evaluation Board for MSP430FG4619 http://www.sparkfun.com/commerce/produc ... ts_id=8298 . So the problem is specific to this board, its code and processor type. This eliminates problems caused by my programmer or my mspgcc install.
When I run msp430-jtag, I get the following error with the parallel programmer http://www.sparkfun.com/commerce/produc ... ucts_id=15:
- I have checked the solder bridges for the OLI/TI selection (see above image).
- I have tried programming with both JTAG and coin cell power with the appropriate jumper setting.
Any ideas as to why this board does not want to be programed?
When I run msp430-jtag, I get the following error with the parallel programmer http://www.sparkfun.com/commerce/produc ... ucts_id=15:
Code: Select all
And this error with the USB http://www.sparkfun.com/commerce/produc ... cts_id=623:
msp430-gcc -g -mmcu=msp430x2013 -o main.elf main.c
msp430-jtag -eE main.elf
MSP430 JTAG programmer Version: 2.3
Use -h for help
Cleaning up after error...
Reset and release device...
An error occoured:
Can't open interface: Could not find device (or device not supported)
Code: Select all
When programming with USB, the red "write" led quickly blinks twice on the programmer. Both methods causes the red led on the Motion Detection Module to turn on dimly. Once the JTAG programing fails, the board resets and goes into the program it was shipped with.msp430-gcc -g -mmcu=msp430x2013 -o main.elf main.c
msp430-jtag -lTIUSB -eE main.elf
MSP430 JTAG programmer Version: 2.3
Use -h for help
Cleaning up after error...
Reset and release device...
An error occoured:
Could not reset target (no connection?): Could not communicate with FET
- I have checked the solder bridges for the OLI/TI selection (see above image).
- I have tried programming with both JTAG and coin cell power with the appropriate jumper setting.
Any ideas as to why this board does not want to be programed?