- Tue Apr 27, 2021 3:50 am
#225370
Hello!
My goal is to have three sperate SPI interfaces on my SAMD51 but I am a bit confused on how to achieve that. So... I have the variant.cpp file in which I configure my pins. As far as I can see, five out of six SERCOMs are in use:
SERCOM0: SPI
SERCOM1: UART
SERCOM2: SPI1
SERCOM3: I2C
SERCOM4: I2C1
SERCOM5: unused(?)
The part I do not understand can be found at the bottom of the variant.cpp:
Serial1 is using the UART pins, configured in the pin description array, isn't it? According to that, it should not use SERCOM5. Am I missing something here? Also: I do not really understand, why Serial1 has four IRQ handlers...
Maybe someone is able to enlighten me. Thanks!
Greetings - Vulpecula
Edit: My Plan was to use SERCOM5 for the third SPI Interface and 'sacrifice' the I2S interface which I don't need. The pins/ports/pads do offer SERCOM5. Also... Am I actually able to use SPI1 in my case or is it internally connected to something else?
My goal is to have three sperate SPI interfaces on my SAMD51 but I am a bit confused on how to achieve that. So... I have the variant.cpp file in which I configure my pins. As far as I can see, five out of six SERCOMs are in use:
SERCOM0: SPI
Code: Select all
{ PORTA, 4, PIO_SERCOM_ALT, PIN_ATTR_DIGITAL, No_ADC_Channel, NOT_ON_PWM, NOT_ON_TIMER, EXTERNAL_INT_11 }, // COPI SERCOM 0 / PAD[0]
{ PORTA, 5, PIO_SERCOM_ALT, PIN_ATTR_DIGITAL, No_ADC_Channel, NOT_ON_PWM, NOT_ON_TIMER, EXTERNAL_INT_12 }, // SCK SERCOM 0 / PAD[1]
{ PORTA, 6, PIO_SERCOM_ALT, PIN_ATTR_DIGITAL, No_ADC_Channel, NOT_ON_PWM, NOT_ON_TIMER, EXTERNAL_INT_13 }, // CIPO SERCOM 0 / PAD[2]
{ PORTA, 7, PIO_SERCOM_ALT, PIN_ATTR_DIGITAL, No_ADC_Channel, NOT_ON_PWM, NOT_ON_TIMER, EXTERNAL_INT_13 }, // CS SERCOM 0 / PAD[3]
SERCOM1: UART
Code: Select all
{ PORTB, 31, PIO_SERCOM_ALT, PIN_ATTR_NONE, No_ADC_Channel, NOT_ON_PWM, TC0_CH0, EXTERNAL_INT_15 }, // 5 UART TX SERCOM 1 / PAD[0]
{ PORTB, 30, PIO_SERCOM_ALT, PIN_ATTR_NONE, No_ADC_Channel, NOT_ON_PWM, TC0_CH0, EXTERNAL_INT_14 }, // 6 UART RX SERCOM 1 / PAD[1]
SERCOM2: SPI1
Code: Select all
{ PORTA, 9, PIO_SERCOM_ALT, PIN_ATTR_DIGITAL, No_ADC_Channel, NOT_ON_PWM, NOT_ON_TIMER, EXTERNAL_INT_1 }, // SPI1 COPI1 SERCOM 2 / PAD[0]
{ PORTA, 8, PIO_SERCOM_ALT, PIN_ATTR_DIGITAL, No_ADC_Channel, NOT_ON_PWM, NOT_ON_TIMER, EXTERNAL_INT_0 }, // SPI1 SCK1 SERCOM 2 / PAD[1]
{ PORTA, 10, PIO_SERCOM_ALT, PIN_ATTR_DIGITAL, No_ADC_Channel, NOT_ON_PWM, NOT_ON_TIMER, EXTERNAL_INT_2 }, // SPI1 CIPO1 SERCOM 2 / PAD[2]
{ PORTA, 11, PIO_SERCOM_ALT, PIN_ATTR_DIGITAL, No_ADC_Channel, NOT_ON_PWM, NOT_ON_TIMER, EXTERNAL_INT_3 }, // SPI1 CS1 SERCOM 2 / PAD[3]
SERCOM3: I2C
Code: Select all
{ PORTA, 16, PIO_SERCOM_ALT, PIN_ATTR_PWM_F, No_ADC_Channel, TCC1_CH0, TC2_CH0, EXTERNAL_INT_0 }, // I2C SCL SERCOM 3 / PAD[1]
{ PORTA, 17, PIO_SERCOM_ALT, PIN_ATTR_PWM_G, No_ADC_Channel, TCC0_CH5, TC2_CH1, EXTERNAL_INT_1 }, // I2C SDA SERCOM 3 / PAD[0]
SERCOM4: I2C1
Code: Select all
{ PORTA, 12, PIO_SERCOM_ALT, PIN_ATTR_PWM_G, No_ADC_Channel, TCC1_CH2, TC2_CH0, EXTERNAL_INT_12 }, // I2C1 SCL1 (RX) SERCOM 4 / PAD[1]
{ PORTA, 13, PIO_SERCOM_ALT, PIN_ATTR_PWM_G, No_ADC_Channel, TCC1_CH3, TC2_CH1, EXTERNAL_INT_13 }, // I2C1 SDA1 (TX) SERCOM 4 / PAD[0]
SERCOM5: unused(?)
The part I do not understand can be found at the bottom of the variant.cpp:
Code: Select all
/* Multi-serial objects instantiation */
SERCOM sercom0(SERCOM0);
SERCOM sercom1(SERCOM1);
SERCOM sercom2(SERCOM2);
SERCOM sercom3(SERCOM3);
SERCOM sercom4(SERCOM4);
SERCOM sercom5(SERCOM5);
Uart Serial1( &sercom5, PIN_SERIAL1_RX, PIN_SERIAL1_TX, PAD_SERIAL1_RX, PAD_SERIAL1_TX ) ;
void SERCOM5_0_Handler() { Serial1.IrqHandler(); }
void SERCOM5_1_Handler() { Serial1.IrqHandler(); }
void SERCOM5_2_Handler() { Serial1.IrqHandler(); }
void SERCOM5_3_Handler() { Serial1.IrqHandler(); }
Serial1 is using the UART pins, configured in the pin description array, isn't it? According to that, it should not use SERCOM5. Am I missing something here? Also: I do not really understand, why Serial1 has four IRQ handlers...
Maybe someone is able to enlighten me. Thanks!
Greetings - Vulpecula
Edit: My Plan was to use SERCOM5 for the third SPI Interface and 'sacrifice' the I2S interface which I don't need. The pins/ports/pads do offer SERCOM5. Also... Am I actually able to use SPI1 in my case or is it internally connected to something else?
Code: Select all
/****** I2S (SDO, SDI, FS, SCK) Pins 40...44 **************************************************************************************/
{ PORTA, 21, PIO_DIGITAL, PIN_ATTR_PWM_F, No_ADC_Channel, TCC0_CH1, TC7_CH0, EXTERNAL_INT_5 }, // SDO SERCOM 5 / PAD[3]
{ PORTA, 22, PIO_DIGITAL, PIN_ATTR_PWM_F, No_ADC_Channel, TCC0_CH2, TC4_CH0, EXTERNAL_INT_6 }, // SDI SERCOM 3 / PAD[0]
{ PORTB, 16, PIO_DIGITAL, PIN_ATTR_PWM_G, No_ADC_Channel, TCC3_CH0, TC4_CH0, EXTERNAL_INT_12 }, // SCK SERCOM 5 / PAD[0]
{ PORTB, 17, PIO_DIGITAL, PIN_ATTR_PWM_F, No_ADC_Channel, TCC3_CH1, TC6_CH1, EXTERNAL_INT_12 }, // MCLK SERCOM 5 / PAD[1]
{ PORTA, 20, PIO_DIGITAL, PIN_ATTR_DIGITAL, No_ADC_Channel, NOT_ON_PWM, NOT_ON_TIMER, EXTERNAL_INT_4 }, // FS SERCOM 5 / PAD[2]