- Wed Apr 21, 2021 11:02 pm
#225254
Hello,
I had some problems choosing the right forum (I am not using the Arduino libraries but the Ambiq SDK alone).
Anyway, here is my problem:
I am trying to port my own RTOS (which already runs on some other M4F-based MCUs) to Apollo3.
As many other RTOSs, I am using the SysTick for Tick generation, and a idle-task, which is basically a
__WFE() loop.
Problem: The Apollo3 does not wake up from sleeping if SysTick interrupts are generated.
I boiled down the problem to the following source code:
everything is working as expected. Two LEDs blinking...
When I use only __WFE in the waiting loop, the LED controlled by SysTick is not blinking any more.
The processor stays in sleep (or some other strange state I am not aware of) , although interrupts
(events) should be generated by SysTick. At least this is working without any problems on other M4F-based MCUs.
Yes, I know that there are various methods in the Ambiq SDK to control the memory power in sleep
states, cache control etc. etc., but up to now I had no success in making this simple setup work.
Another strange thing is, that if I attach a debugger (Ozone) to the not-working program via a Segger JLink,
the LED starts blinking. I suspect that the debug events make a change somehow. When I disconnect the
debugger, the LED stops blinking again.
I am using a Artemis Nano Board, btw.
So what is going wrong here? What do I have to do to wake up Apollo3 from sleep via SysTick interrupts?
Any help is welcome!
Andreas
I had some problems choosing the right forum (I am not using the Arduino libraries but the Ambiq SDK alone).
Anyway, here is my problem:
I am trying to port my own RTOS (which already runs on some other M4F-based MCUs) to Apollo3.
As many other RTOSs, I am using the SysTick for Tick generation, and a idle-task, which is basically a
__WFE() loop.
Problem: The Apollo3 does not wake up from sleeping if SysTick interrupts are generated.
I boiled down the problem to the following source code:
Code: Select all
When I have a active waiting loop (comment out WFE and commenting in the other two lines), #include "am_mcu_apollo.h"
void SysTick_Handler(void) {
am_hal_gpio_state_write(13, AM_HAL_GPIO_OUTPUT_TOGGLE);
}
int main(void)
{
const am_hal_gpio_pincfg_t config13 = {
.uFuncSel = AM_HAL_PIN_13_GPIO,
.eDriveStrength = AM_HAL_GPIO_PIN_DRIVESTRENGTH_12MA,
.eGPOutcfg = AM_HAL_GPIO_PIN_OUTCFG_PUSHPULL,
.eGPInput = AM_HAL_GPIO_PIN_INPUT_NONE
};
const am_hal_gpio_pincfg_t config19 = {
.uFuncSel = AM_HAL_PIN_19_GPIO,
.eDriveStrength = AM_HAL_GPIO_PIN_DRIVESTRENGTH_12MA,
.eGPOutcfg = AM_HAL_GPIO_PIN_OUTCFG_PUSHPULL,
.eGPInput = AM_HAL_GPIO_PIN_INPUT_NONE
};
am_hal_gpio_pinconfig(13, config13);
am_hal_gpio_pinconfig(19, config19);
SysTick_Config(SystemCoreClock / 5);
while(1) {
__WFE();
// am_hal_gpio_state_write(19, AM_HAL_GPIO_OUTPUT_TOGGLE);
// for (int i=0; i < 100000; ++i) ;
}
}
everything is working as expected. Two LEDs blinking...
When I use only __WFE in the waiting loop, the LED controlled by SysTick is not blinking any more.
The processor stays in sleep (or some other strange state I am not aware of) , although interrupts
(events) should be generated by SysTick. At least this is working without any problems on other M4F-based MCUs.
Yes, I know that there are various methods in the Ambiq SDK to control the memory power in sleep
states, cache control etc. etc., but up to now I had no success in making this simple setup work.
Another strange thing is, that if I attach a debugger (Ozone) to the not-working program via a Segger JLink,
the LED starts blinking. I suspect that the debug events make a change somehow. When I disconnect the
debugger, the LED stops blinking again.
I am using a Artemis Nano Board, btw.
So what is going wrong here? What do I have to do to wake up Apollo3 from sleep via SysTick interrupts?
Any help is welcome!
Andreas