- Sat Apr 08, 2017 3:34 pm
#194321
Hi folks,
I have been attempting to program an ESP32. Given the state of the Arduino-like libraries, I downloaded the 2.0 final version of the ESP-IDF onto an Ubuntu 16.04 box.
I have tried the HTTP request and the mDNS examples. Neither one connects to WIFI reliably.
I try the command
make flash monitor
If I do get a connection, it is after an initial flashing. However, if I hit the reset button on the ESP, or perhaps try reflashing, it will often not connect to WIFI. I have also seen a lot of garbled output from the examples when they do work, some of the text I expect to see and then something that looks like some non-ASCII data was part of the print attempt.
Anyone else run into these problems?
Thanks!
-Keith
I have been attempting to program an ESP32. Given the state of the Arduino-like libraries, I downloaded the 2.0 final version of the ESP-IDF onto an Ubuntu 16.04 box.
I have tried the HTTP request and the mDNS examples. Neither one connects to WIFI reliably.
I try the command
make flash monitor
If I do get a connection, it is after an initial flashing. However, if I hit the reset button on the ESP, or perhaps try reflashing, it will often not connect to WIFI. I have also seen a lot of garbled output from the examples when they do work, some of the text I expect to see and then something that looks like some non-ASCII data was part of the print attempt.
Anyone else run into these problems?
Thanks!
-Keith