- Sat Dec 17, 2011 8:36 am
#137113
Hi All,
I am having trouble building a project in the Eclipse IDE (OPENOCD) to use the I2C, I am using the ST standard library, the olimex ARM-USB-OCD JTAG and the Olimex H103 board with STM32F103 chip. After a lot of tweaking around after receiving many errors, building now seems to fail with only the below error (many of it though!):
I had worked the board with USART with no problems, I am not sure why the I2C is such a trouble!
Help very much appreciated
I am having trouble building a project in the Eclipse IDE (OPENOCD) to use the I2C, I am using the ST standard library, the olimex ARM-USB-OCD JTAG and the Olimex H103 board with STM32F103 chip. After a lot of tweaking around after receiving many errors, building now seems to fail with only the below error (many of it though!):
Code: Select all
After some searching, I found people recommending including the file "stm32f10x_conf.h" in every ".c" file, which didn't sound right for me, and didn't work as well! I have found though that the definition for this "assert_param" is mentioned in the "stm32f10x_conf.h" file as:D:\OlimexODS\projects_STM32\STM32-H103_flash-I2C/lib/stm32f10x_i2c.c:165: undefined reference to `assert_param'
main.o: In function `I2C_Init':
D:\OlimexODS\projects_STM32\STM32-H103_flash-I2C/lib/stm32f10x_i2c.c:198: undefined reference to `assert_param'
D:\OlimexODS\projects_STM32\STM32-H103_flash-I2C/lib/stm32f10x_i2c.c:199: undefined reference to `assert_param'
D:\OlimexODS\projects_STM32\STM32-H103_flash-I2C/lib/stm32f10x_i2c.c:200: undefined reference to `assert_param'
D:\OlimexODS\projects_STM32\STM32-H103_flash-I2C/lib/stm32f10x_i2c.c:201: undefined reference to `assert_param'
main.o:D:\OlimexODS\projects_STM32\STM32-H103_flash-I2C/lib/stm32f10x_i2c.c:202: more undefined references to `assert_param' follow
make: *** [main.out] Error 1
Code: Select all
As i said, I tried including the file, but it still insists that it's "undefined reference" #ifdef DEBUG
/*******************************************************************************
* Macro Name : assert_param
* Description : The assert_param macro is used for function's parameters check.
* It is used only if the library is compiled in DEBUG mode.
* Input : - expr: If expr is false, it calls assert_failed function
* which reports the name of the source file and the source
* line number of the call that failed.
* If expr is true, it returns no value.
* Return : None
*******************************************************************************/
#define assert_param(expr) ((expr) ? (void)0 : assert_failed((u8 *)__FILE__, __LINE__))
/* Exported functions ------------------------------------------------------- */
void assert_failed();//u8* file, u32 line);
#else
#define assert_param(expr) ((void)0)
#endif /* DEBUG */
I had worked the board with USART with no problems, I am not sure why the I2C is such a trouble!
Help very much appreciated