- Wed Oct 19, 2011 6:14 am
#134789
Hi guys,
I recently succeeded in updating the Geiger Counter (http://www.sparkfun.com/products/9848) firmware to v13. I a total novice with AVR Studio so doing this is a real achievement.
But I searched the net and realized that the counter should output counts per minute instead of counts per second (as available with v13) as to be able to really understand the output and properly compare it with other people and the accepted limit. See: https://pachube.com/feeds?tag=radiation
Anyone willing to modify it in order to output counts per minute? Or any suggestions?
Thank you,
zws
Here is the code (v13) supplied by Aaron Weiss at: https://github.com/a1ronzo/SparkFun-Gei ... its/master
I recently succeeded in updating the Geiger Counter (http://www.sparkfun.com/products/9848) firmware to v13. I a total novice with AVR Studio so doing this is a real achievement.
But I searched the net and realized that the counter should output counts per minute instead of counts per second (as available with v13) as to be able to really understand the output and properly compare it with other people and the accepted limit. See: https://pachube.com/feeds?tag=radiation
Anyone willing to modify it in order to output counts per minute? Or any suggestions?
Thank you,
zws
Here is the code (v13) supplied by Aaron Weiss at: https://github.com/a1ronzo/SparkFun-Gei ... its/master
Code: Select all
/*
9-1-09
Aaron Weiss
Geiger Counter
v13: displays counts per second, every second
Internal 8MHz: lfuse = 0xE2, hfuse = 0xDF
*/
#include <stdlib.h>
#include <stdio.h>
#include <avr/io.h>
#include <avr/pgmspace.h>
#include <avr/interrupt.h>
#define FOSC 8000000
#define BAUD 9600
#define MYUBRR 51
#define sbi(var, mask) ((var) |= (uint8_t)(1 << mask))
#define cbi(var, mask) ((var) &= (uint8_t)~(1 << mask))
#define STATUS_LED 5
//uint16_t global_clock;
volatile long i=0;
///============Initialize Prototypes=====================///////////////////////
void ioinit(void); // initializes IO
static int uart_putchar(char c, FILE *stream);
uint8_t uart_getchar(void);
static FILE mystdout = FDEV_SETUP_STREAM(uart_putchar, NULL, _FDEV_SETUP_WRITE);
void delay_ms(uint16_t x); // general purpose delay
/////===================================================////////////////////////
ISR (INT0_vect)
{
i++;
cbi(PORTC, STATUS_LED);
}
ISR(TIMER1_OVF_vect)
{
TCNT1 = 34000; //(256/8MHz)*(65536bits-34000)~=1.009s
printf("counts per second: %ld \r", i);
i=0;
}
//=========MAIN================/////////////////////////////////////////////////
int main(void)
{
ioinit(); //Setup IO pins and defaults
delay_ms(1200); //wait to settle
while(1)
{
sbi(PORTC, STATUS_LED);
delay_ms(30);
}
cli();
}
////////////////////////////////////////////////////////////////////////////////
///==============Initializations=======================================/////////
////////////////////////////////////////////////////////////////////////////////
void ioinit (void)
{
//1 = output, 0 = input
DDRB = 0b11101111; //PB4 = MISO
DDRC = 0b00110001; //Output on PORTC0, PORTC4 (SDA), PORTC5 (SCL), all others are inputs
DDRD = 0b11110010; //PORTD (RX on PD0), input on PD2
//USART Baud rate: 9600
UBRR0H = MYUBRR >> 8;
UBRR0L = MYUBRR;
UCSR0B = (1<<RXEN0)|(1<<TXEN0);
stdout = &mystdout; //Required for printf init
//pin change interrupt on INT0
EICRA = (1<<ISC01);//falling edge generates interrupt
EIMSK = (1<<INT0);
// Setting Timer 1:
// normal mode
TCCR1A = 0x00;
// Set to clk/256
TCCR1B |= (1<<CS12);
//enable overflow interrupt
TIMSK1 |= (1<<TOIE1);
//load timer with a value to optimize for 1 second, (256/8MHz)*(65536bits-34000)~=1.009s
TCNT1 = 34000;
sei(); //turn on global interrupts
}
static int uart_putchar(char c, FILE *stream)
{
if (c == '\n') uart_putchar('\r', stream);
loop_until_bit_is_set(UCSR0A, UDRE0);
UDR0 = c;
return 0;
}
uint8_t uart_getchar(void)
{
while( !(UCSR0A & (1<<RXC0)) );
return(UDR0);
}
//General short delays
void delay_ms(uint16_t x)
{
uint8_t y, z;
for ( ; x > 0 ; x--){
for ( y = 0 ; y < 40 ; y++){
for ( z = 0 ; z < 40 ; z++){
asm volatile ("nop");
}
}
}
}