- Thu Dec 09, 2010 8:53 pm
#115268
I've been messing around with the Arduino, systematically plugging it into whatever I have around and trying to get it to work. My wife calls this "nerding-out time." I can't totally disagree with her. I digress...
I had some 1Kbit 24LC01B EEPROMs lying around and I couldn't figure out how to program them. I finally busted out my scope and got it to work. I still don't quite understand how it does work because I don't see how the read bit ever gets set, but I'm not going to look a gift horse in the mouth.
Here's the Arduino code in case I can save anyone else any time.
I had some 1Kbit 24LC01B EEPROMs lying around and I couldn't figure out how to program them. I finally busted out my scope and got it to work. I still don't quite understand how it does work because I don't see how the read bit ever gets set, but I'm not going to look a gift horse in the mouth.
Here's the Arduino code in case I can save anyone else any time.
Code: Select all
#include <Wire.h>
/*
Wire Hookup for 24LC01B 1 K-bit (128 byte) EEPROM
Don't forget to read the datasheet!
http://ww1.microchip.com/downloads/en/devicedoc/21711c.pdf
1,2,3 are not internally connected.
It's okay to leave them open.
-----
-|1 8|- Arduino +5V
-|2 7|- Jumper to +5V for Write Protect
-|3 6|- Arduino Pin Analog-5
Arduino Gnd -|4 5|- Arduino Pin Analog-4
-----
I put a 2.2K pull-up resistor between pin 5 and 8
because the datasheet suggested it, but I'm not entirely
sure it's necessary as I think the Wire library enables
the Arduino's internal pull-ups. Don't quote me on that,
though.
You're supposed to be able to write 8 bytes at
a time, but I had trouble with that. Try 4 at
a time with a delay and then push it up until
your results degrade.
It seems like you can read as many as you like.
We're going to write Hello World!
Data |H|e|l|l|o| |W|o|r|l|d|!|
|-|-|-|-|-|-|-|-|-|-|-|-|
Address |0|1|2|3|4|5|6|7|8|9|1|1|
| | | | | | | | | | |0|1|
*/
void setup()
{
Wire.begin(); // join i2c bus (address optional for master)
Serial.begin(9600);
}
void loop()
{
Serial.println("Writing...");
Wire.beginTransmission(0x50); // This is the 24LC01B device address
Wire.send(0x0); // Start writing at address 0
Wire.send("Hell"); // Send 4 bytes
Wire.endTransmission();
delay(10); // Without a short delay, the EEPROM is still
// writing when you start to write the next block
// Feel free to experiment with the delay length
Wire.beginTransmission(0x50);
Wire.send(0x4); // Write next four bytes starting at address 4
Wire.send("o Wo");
Wire.endTransmission();
delay(10);
Wire.beginTransmission(0x50);
Wire.send(0x8); // Write last four bytes starting at address 8
Wire.send("rld!");
Wire.endTransmission();
delay(10);
Serial.println("Reading...");
Wire.beginTransmission(0x50); // Now we're going to read it back
Wire.send(0x0); // Sending address 0, so it knows where we'll want
Wire.endTransmission(); // to read from
Wire.requestFrom(0x50,12); // Start new transmission and keep reading for 12 bytes
while(Wire.available())
{
char c = Wire.receive(); // Read a byte and write it out to the Serial port
Serial.print(c);
}
Serial.println();
delay(5000);
}