- Sat Nov 03, 2018 10:48 pm
#200867
Hey all I am having the hardest time trying to figure out how to go about the order of decryption the encrypted text.
This is my sketch code:
Help would be great in order to solve this issue!
This is my sketch code:
Code: Select all
And this is the output I get:#include "AES.h"
#include "base64.h"
AES aes;
void gen_iv(byte *iv) {
for (int i = 0 ; i < N_BLOCK ; i++ ) {
iv[i]= (byte) *(volatile uint8_t *)0x3FF20E44;
}
}
void setup() {
Serial.begin(115200);
Serial.println("\nBooting...");
char b64data[2000];
byte cipher[1000];
byte iv [N_BLOCK];
char *encodedFinal;
Serial.println("Let's encrypt:");
byte *key = (unsigned char*)"5TGB&YHN7UJM(IK<";
byte *my_iv = (unsigned char*)"!QAZ2WSX#EDC4RFV";
char *msg = "{\"data\":{\"value\":300}, \"SEQN\":700 , \"msg\":\"IT WORKS!!\" }";
//Set the key for AES
aes.set_key(key, sizeof(key));
/*
==================================================================
Encoding section
==================================================================
*/
//Encode IV to Base64
base64_encode(b64data, (char *)my_iv, N_BLOCK);
Serial.println(" IV -> Base64: " + String(b64data));
Serial.println(" Orignal Msg: " + String(msg));
//Encode message into Base64
int b64len = base64_encode(b64data, (char *)msg, String(msg).length());
Serial.println(" Message -> Base64: " + String(b64data));
// Encrypt into AES256
aes.do_aes_encrypt((byte *)b64data, b64len , cipher, key, 256, my_iv);
Serial.println("Encrypted: " + String(b64data));
//Encode everything now in Base64
base64_encode(b64data, (char *)cipher, aes.get_size());
Serial.println("Encrypted -> Base64: " + String(b64data));
encodedFinal = (char*)b64data;
Serial.println("Final encoded: " + String(encodedFinal));
/*
==================================================================
Decoding section
==================================================================
*/
Serial.println();
Serial.println();
Serial.println();
Serial.println();
//Decoding everything from Base64
char b64dataDecode[2000];
byte cipherDecode[1000];
//Decode from Base64 to Encrypted msg
base64_decode(b64dataDecode, (char *)encodedFinal, aes.get_size());
Serial.println(" Base64 -> Encrypted: " + String(b64dataDecode));
//Decoding from Encrypted
aes.do_aes_decrypt((byte *)encodedFinal, base64_dec_len(encodedFinal, String(encodedFinal).length()), cipherDecode, key, 256, my_iv);
Serial.println("Encrypted -> Original Msg: ") + String(encodedFinal);
Serial.println("Done...");
}
void loop() {
// put your main code here, to run repeatedly:
}
Booting...As you can see above, the decryption is not working correctly. The encryption works just fine though (but i think the Encoding part is not coming out correctly since its the same as the Base64 encoding?).
Let's encrypt:
IV -> Base64: IVFBWjJXU1gjRURDNFJGVg==
Orignal Msg: {"data":{"value":300}, "SEQN":700 , "msg":"IT WORKS!!" }
Message -> Base64: eyJkYXRhIjp7InZhbHVlIjozMDB9LCAiU0VRTiI6NzAwICwgIm1zZyI6IklUIFdPUktTISEiIH0=
Encrypted: eyJkYXRhIjp7InZhbHVlIjozMDB9LCAiU0VRTiI6NzAwICwgIm1zZyI6IklUIFdPUktTISEiIH0=
Encrypted -> Base64: sD9f8LnxQrlOvTODLbzXPM5wWMk6+KnpmGiowTtKswGK80+yf9DyHjjiF94TwUpP/1V4f9KsHA7+1oAmBy12Dl8Dvk/ZclFvNeNrXSwCFlU=
Final encoded: sD9f8LnxQrlOvTODLbzXPM5wWMk6+KnpmGiowTtKswGK80+yf9DyHjjiF94TwUpP/1V4f9KsHA7+1oAmBy12Dl8Dvk/ZclFvNeNrXSwCFlU=
Base64 -> Encrypted: ⸮?_⸮⸮B⸮N⸮3⸮-⸮⸮<⸮pX⸮:⸮⸮⸮h⸮⸮;J⸮⸮⸮O⸮⸮⸮8⸮⸮⸮JO⸮UxҬ⸮ր&
Encrypted -> Original Msg:
Done...
Help would be great in order to solve this issue!