- Wed Nov 29, 2006 9:14 am
#22712
Hey guys. I am now working on a wireless protocol to use with the Nordic 24L01 chips. I want to do some encryption, but I have never studied actual encryption algorithms. I have used the cryptography library with .NET in C#, but that doesn't help me much when it comes to the embedded side of things. Do any of you guys have any suggestions on what algorithms would be good to use in embedded applications? Any links would also be really helpful. Thanks.
FYI - I'm using a Philips LPC2148 ARM7 uC, which has (IIRC) 40 kB of RAM and runs at 60 MHz. The Nordic chip is transmitting data at 2 Mbps.
FYI - I'm using a Philips LPC2148 ARM7 uC, which has (IIRC) 40 kB of RAM and runs at 60 MHz. The Nordic chip is transmitting data at 2 Mbps.