- Fri Jan 04, 2008 5:12 am
#40402
I'm wondering if I can drive these Luxeon LED's directly from an AVR microcontroller, or should I use a transistor?
Where electronics enthusiasts find answers.
azog wrote:The LED says 350mA peak; the AVR I have in mind can source 40mA directly off a port pin.Didn't you just answer your own question?
NleahciM wrote:Yea, but I was hoping to get a different answer than the one I gave myself.azog wrote:The LED says 350mA peak; the AVR I have in mind can source 40mA directly off a port pin.Didn't you just answer your own question?
daemondust wrote:http://i18.tinypic.com/6prgm5s.pngI would not recommend driving a Luxeon with a ballast resistor. At 350mA and a 5V source you will be dissipating about half a watt in the resistor which is very inefficient. If you are using a 7805 as a power source, you will also dissipate a lot of power there too since it is a linear component.