- Thu Nov 01, 2007 11:42 pm
#37415
This is regarding a wireless logger application: My final target application would require very small size of the part that will transmit data most of the time and will require a ceramic chip antenna; the receiving download station could be bigger and accept a duck antenna, at least 10cm long, perhaps even 20cm length. I only need short range of 10-20cm, however the medium transmitted through will not be very favorable, in fact the first goal will be to determine if it is possible at all at this frequency.
I have read some of the threads like this one,
viewtopic.php?t=6353&highlight=mirf++umirf which indicates that nRF24L01 is a better chip than nRF2401A. However I am uncertain about the short range reported for the MiRF v2 with ceramic chip antenna. Size is also an issue, however the board of MiRF v2 should be just acceptable. Power consumption in the logger/transmitter part would be very important due to small size and low battery capacity.
So how would two uMiRF's measure up against a pair of MiRF v2, one with ceramic chip and the other with duck antenna?
I have read some of the threads like this one,
viewtopic.php?t=6353&highlight=mirf++umirf which indicates that nRF24L01 is a better chip than nRF2401A. However I am uncertain about the short range reported for the MiRF v2 with ceramic chip antenna. Size is also an issue, however the board of MiRF v2 should be just acceptable. Power consumption in the logger/transmitter part would be very important due to small size and low battery capacity.
So how would two uMiRF's measure up against a pair of MiRF v2, one with ceramic chip and the other with duck antenna?