It should wait but doesn't (it's not you), actually I'm a bit annoyed that I couldn't find exactly why, although printing the offending serial input suggests there are stray line feed/carriage returns being sent by the Arduino Serial Monitor.
Here's some code that works, with a serial timeout function which may be useful if you want to have the option of skipping past the data entry:
Code: Select all/* Author: Nathan Seidle
Created: June 12th, 2019
License: MIT. See SparkFun Arduino Apollo3 Project for more information
This example demonstrates usage of:
Serial
Serial1
This example works best on the BlackBoard Artemis and BlackBoard Artemis ATP that have
the TX1 and RX1 pins exposed. See the advanced serial example for setting up a serial
port on other pins and other carrier boards.
*/
bool waitForSerialIncTimeout(uint32_t timeout = 20000)
{
uint32_t startTime;
if(timeout == 0)
startTime = 0xFFFFFFFF; //Highest possible value, effectively preventing timeout
else
startTime = millis();
while(Serial.available()) Serial.read();
delay(50);
while (!Serial.available() && millis() < startTime+timeout)
{
delay(1000);
Serial.print(".");
} //Wait for input
Serial.println();
if(Serial.available())
return true;
else
{
Serial.println("Wait for input timed out");
return false;
}
}
void setup()
{
Serial.begin(9600);
Serial.println("Hello debug window!");
Serial1.begin(115200);
Serial1.println("This prints on TX1/RX1 pins");
}
void loop()
{
Serial.println("Time for a menu:");
Serial.println("a) Activate the cheese");
Serial.println("x) Exit");
Serial.println();
waitForSerialIncTimeout(0);
char incoming = Serial.read();
if (incoming == 'a' || incoming == 'A')
{
Serial.println("How many cheeses to dispense?");
waitForSerialIncTimeout(0);
delay(100);
unsigned int cheeseCount = Serial.parseInt(); //That's a lot of potential cheese
//Print to second serial port
for (unsigned int x = 0; x < cheeseCount; x++)
{
Serial1.println("Cheese!");
}
Serial.printf("Thank you. %d cheeses dispensed.\n\r", cheeseCount); //Did you see that?! We used printf!
}
else if (incoming == 'x' || incoming == 'X')
{
Serial.println("Exiting... Have a nice day.");
while (1)
; //Freeze
}
else
{
Serial.print("Unknown choice: ");
Serial.write(incoming);
Serial.println();
}
}