Thanks for the insights. Everything checks out. I was able to get 20 pins using interrupts without any cross-talk.
In case it helps someone else, I'm sharing my ugly brute-force sketch that creates an interrupt routine for each of 20 pins. I tested by using a jumper wire from ground to each of these pins one-by-one to ensure only the counter for the respective pin is incrementing. Previously (on a Metro M0 Express board), pins shared underlying ISR's, causing PinA's toggle to increment Pin B's counter. That wasn't fun -- for the longest time I thought I had a hardware short or brownout issue from encoders.
Code: Select all/*
Brute force check to ensure hardware interrupts aren't cross-talking. Tested with a jumper from ground, then going one-by one down the pins.
Listed here in order they are phyisically on the board. Starting nearest the usb plug and moving down, but skipping pins w/o numbers. Then a few on the left (I needed 20).
Going down the list twice and watching the counts, I confirmed no Pin's count was being incremented by another pin (a problem I had with Metro M0 boards).
*/
int count_13=0;
int count_12=0;
int count_32=0;
int count_28=0;
int count_27=0;
int count_23=0;
int count_22=0;
int count_04=0;
int count_35=0;
int count_14=0;
int count_08=0;
int count_10=0;
int count_09=0;
int count_26=0;
int count_15=0;
int count_19=0;
int count_18=0;
int count_17=0;
int count_41=0;
int count_45=0;
// defines pin number on the board (not the pin's current value)
int Pin_13=13;
int Pin_12=12;
int Pin_32=32;
int Pin_28=28;
int Pin_27=27;
int Pin_23=23;
int Pin_22=22;
int Pin_04=4;
int Pin_35=35;
int Pin_14=14;
int Pin_08=8;
int Pin_10=10;
int Pin_09=9;
int Pin_26=26;
int Pin_15=15;
int Pin_19=19;
int Pin_18=18;
int Pin_17=17;
int Pin_41=41;
int Pin_45=45;
void setup() {
//start serial connection
Serial.begin(9600);
//configure as an input and enable the internal pull-up resistor
pinMode(13, INPUT_PULLUP);
pinMode(12, INPUT_PULLUP);
pinMode(32, INPUT_PULLUP);
pinMode(28, INPUT_PULLUP);
pinMode(27, INPUT_PULLUP);
pinMode(23, INPUT_PULLUP);
pinMode(22, INPUT_PULLUP);
pinMode(4, INPUT_PULLUP);
pinMode(35, INPUT_PULLUP);
pinMode(14, INPUT_PULLUP);
pinMode(8, INPUT_PULLUP);
pinMode(10, INPUT_PULLUP);
pinMode(9, INPUT_PULLUP);
pinMode(26, INPUT_PULLUP);
pinMode(15, INPUT_PULLUP);
pinMode(19, INPUT_PULLUP);
pinMode(18, INPUT_PULLUP);
pinMode(17, INPUT_PULLUP);
pinMode(41, INPUT_PULLUP);
pinMode(45, INPUT_PULLUP);
pinMode(5, OUTPUT);
attachInterrupt(digitalPinToInterrupt(Pin_13), myIntRoutine_13, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_12), myIntRoutine_12, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_32), myIntRoutine_32, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_28), myIntRoutine_28, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_27), myIntRoutine_27, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_23), myIntRoutine_23, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_22), myIntRoutine_22, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_04), myIntRoutine_04, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_35), myIntRoutine_35, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_14), myIntRoutine_14, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_08), myIntRoutine_08, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_10), myIntRoutine_10, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_09), myIntRoutine_09, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_26), myIntRoutine_26, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_15), myIntRoutine_15, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_19), myIntRoutine_19, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_18), myIntRoutine_18, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_17), myIntRoutine_17, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_41), myIntRoutine_41, RISING);
attachInterrupt(digitalPinToInterrupt(Pin_45), myIntRoutine_45, RISING);
}
void loop() {
Serial.println("I still exist...");
delay(2000);
}
////////////////////
// Create interrupt routine for each pin...
void myIntRoutine_13(){
count_13++;
Serial.print("_13 Within the ISR; count value ->");
Serial.println(count_13);
}
void myIntRoutine_12(){
count_12++;
Serial.print("_12 Within the ISR; count value ->");
Serial.println(count_12);
}
void myIntRoutine_32(){
count_32++;
Serial.print("_32 Within the ISR; count value ->");
Serial.println(count_32);
}
void myIntRoutine_28(){
count_28++;
Serial.print("_28 Within the ISR; count value ->");
Serial.println(count_28);
}
void myIntRoutine_27(){
count_27++;
Serial.print("_27 Within the ISR; count value ->");
Serial.println(count_27);
}
void myIntRoutine_23(){
count_23++;
Serial.print("_23 Within the ISR; count value ->");
Serial.println(count_23);
}
void myIntRoutine_22(){
count_22++;
Serial.print("_22 Within the ISR; count value ->");
Serial.println(count_22);
}
void myIntRoutine_04(){
count_04++;
Serial.print("_04 Within the ISR; count value ->");
Serial.println(count_04);
}
void myIntRoutine_35(){
count_35++;
Serial.print("_35 Within the ISR; count value ->");
Serial.println(count_35);
}
void myIntRoutine_14(){
count_14++;
Serial.print("_14 Within the ISR; count value ->");
Serial.println(count_14);
}
void myIntRoutine_08(){
count_08++;
Serial.print("_08 Within the ISR; count value ->");
Serial.println(count_08);
}
void myIntRoutine_10(){
count_10++;
Serial.print("_10 Within the ISR; count value ->");
Serial.println(count_10);
}
void myIntRoutine_09(){
count_09++;
Serial.print("_09 Within the ISR; count value ->");
Serial.println(count_09);
}
void myIntRoutine_26(){
count_26++;
Serial.print("_26 Within the ISR; count value ->");
Serial.println(count_26);
}
void myIntRoutine_15(){
count_15++;
Serial.print("_15 Within the ISR; count value ->");
Serial.println(count_15);
}
void myIntRoutine_19(){
count_19++;
Serial.print("_19 Within the ISR; count value ->");
Serial.println(count_19);
}
void myIntRoutine_18(){
count_18++;
Serial.print("_18 Within the ISR; count value ->");
Serial.println(count_18);
}
void myIntRoutine_17(){
count_17++;
Serial.print("_17 Within the ISR; count value ->");
Serial.println(count_17);
}
void myIntRoutine_41(){
count_41++;
Serial.print("_41 Within the ISR; count value ->");
Serial.println(count_41);
}
void myIntRoutine_45(){
count_45++;
Serial.print("_45 Within the ISR; count value ->");
Serial.println(count_45);
}