PIR switch/fade in fade out combo to activate LED strip lighting

General project discussion / help
Did you make a robotic coffee pot which implements HTCPCP and decafs unauthorized users? Show it off here!

Moderator: phalanx

Post Reply
Gwmilne
Posts: 1
Joined: Sun Sep 09, 2018 4:37 pm

PIR switch/fade in fade out combo to activate LED strip lighting

Post by Gwmilne » Sun Sep 09, 2018 6:48 pm

Hello. I’m a full time artist (25 years) and am working on a series of large optical wall sculptures (typical 60” x 30” x 3” depth) that require 6-10A of LED strip lighting. I’d like to activate the lighting using a PIR switch, and would like the LEDs to fade on (20-30 seconds) and fade off (same amount of time). My clients are demanding. I need the mechanism(s) to be robust, lasting hopefully as long as the LED lights (50,000 hours or so). I produce approximately 1 piece per month so I also need to be able to replicate the mechanism. Any help would be greatly appreciated. PS. I’ve purchased the Oznium dimmer for tests but it’s 2A max makes its use in actual pieces unfeasible.

xtonybaloneyx
Posts: 1
Joined: Fri Nov 09, 2018 9:37 am

Re: PIR switch/fade in fade out combo to activate LED strip lighting

Post by xtonybaloneyx » Fri Nov 09, 2018 9:40 am

Hey Curious if you ever found a solution to this problem? Im in the same situation myself. That dimmer you posted is a perfect size for me but it need it to function automatically as well. Any tips would be greatly appreciated.

- tony

Post Reply