ESP32 Thing not on network (does not acknowledge ping)

All things pertaining to wireless and RF links

Moderator: phalanx

Post Reply
femtosystems
Posts: 1
Joined: Mon Jul 02, 2018 6:51 am

ESP32 Thing not on network (does not acknowledge ping)

Post by femtosystems » Mon Jul 02, 2018 7:45 am

* Updated the Arduino ESP32 libraries via github to the latest and greatest
* Using "HelloServer" sketch (from Examples->WebServer->HelloServer)
* Tested (2) SparkFun ESP32 Things and (1) DFRobot ESP32 FireBeetle using above sketch (i.e. "HelloServer")
* Both ESP32 Things will not answer a generic "ping" request
* FireBeetle respnds to the "ping" request
* RSSI on all three boards between -54 and -56 (checked with WiFi.scanNetworks() in a different sketch

Attached: 3 snapshots: 192.168.1.107 and 192.168.1.103 are ESP32 Things. 192.168.1.102 is a FireBeetle

==> why do the ESP32 Things indicate that they are connected to the network but cannot receive a simple ping?
==> no issues with FireBeetle using identical environment so the finger is pointing towards the ESP32 Thing as the problem

Image
Image
Image

paulvha
Posts: 222
Joined: Sat Nov 11, 2017 2:39 am

Re: ESP32 Thing not on network (does not acknowledge ping)

Post by paulvha » Sat Jul 07, 2018 11:12 am

Ping is (very) low level implementation in the TCP stack. A basic question: did the helloserver.ino displayed the TCP/IP addresses that you use ? what happens if you connect ? did you get the messages ?

Post Reply