Pi Servo Hat with RPi_Cam_Web_Interface

Have questions about a SparkFun product or board? This is the place to be.

Moderators: phalanx, TS-Tim

Post Reply
impartit
Posts: 4
Joined: Sat Oct 25, 2014 3:59 pm

Pi Servo Hat with RPi_Cam_Web_Interface

Post by impartit » Mon Jun 11, 2018 1:56 am

I am using a "Sparkfun Pi Servo Hat" and cannot figure out how the pan and tilt button outputs of (servo_up(), servo_down() etc.) are handled by the web interface once pipan_off has been renamed to pipan_on, the pipe FIFO_pantilt has been created and the access permissions changed to 666 . Further pipan.php references the servoblaster installation directory and servo_off is the default !!!

The contents of pipan_bak.txt do not change from the one line entry of 90 100.

How do the pan and tilt buttons interact with pantilt.py installed as directed in this URL https://learn.sparkfun.com/tutorials/se ... ilt-camera.

Servos buzz and scoping the signal pins of either show a continuos pulse which does NOT change when a pan or tilt button is pressed.

RHTizzy
Posts: 2
Joined: Sun Jun 24, 2018 10:19 am

Re: Pi Servo Hat with RPi_Cam_Web_Interface

Post by RHTizzy » Sun Jun 24, 2018 10:45 am

Not to hijack your thread but nobody's responded to your call yet and I've the (probably) same problem here: on startup, servo deflection is minimal and then when the pipe is opened by the pi, it seems like the servo's just buzz but actually they're maxed out and still pushing which gets them really hot and would probably cause them to burn out if left for more than a few seconds or what. Nothing changes when pressing the pan/tilt arrows on the website.

I moved the addressing in pantilt.py to the third and fourth channels which I believe someone recommended in the tutorial you linked, but the same result ensues so no success.

It seems like the pulses expected by the servo's are way different than the hat is configured for. I've used four different servo's with the same result so having a hard time believing they're broken. They are 'old' servo's though (2013ish) so perhaps something with the tech has changed radically since I last used them?

I did try to make sense of https://learn.sparkfun.com/tutorials/pi ... 1521732247 and writing values to the PWM registers but it's all new to me so having a hard time trying to troubleshoot.

All input is welcome!

impartit
Posts: 4
Joined: Sat Oct 25, 2014 3:59 pm

Re: Pi Servo Hat with RPi_Cam_Web_Interface

Post by impartit » Mon Jun 25, 2018 5:56 am

Not hijacking at all and thanks for your response. I am still looking for a solution and would therefore be pleased to hear of any solution that you or others may come up with.

RHTizzy
Posts: 2
Joined: Sun Jun 24, 2018 10:19 am

Re: Pi Servo Hat with RPi_Cam_Web_Interface

Post by RHTizzy » Fri Jun 29, 2018 5:27 am

No response on the Sparkfun comments section either, last time I buy something from them

impartit
Posts: 4
Joined: Sat Oct 25, 2014 3:59 pm

Re: Pi Servo Hat with RPi_Cam_Web_Interface

Post by impartit » Fri Jun 29, 2018 5:46 am

Have you tried using pipan without the servoblaster. I understand all that is required is to rename pipan_off to pipan_off and revert to scan_off if necessary

darrellg
Posts: 328
Joined: Fri Oct 17, 2014 10:02 am
Location: Southern California

Re: Pi Servo Hat with RPi_Cam_Web_Interface

Post by darrellg » Fri Jun 29, 2018 8:51 am

if you want a response from Sparkfun, then you should probably use the actual Sparkfun support page at https://www.sparkfun.com/technical_assistance.

Post Reply