SparkFun Forums 

Where electronics enthusiasts find answers.

By tonyr
#199023
Good morning/ Afternoon

I am working on a project with my son which requires measurement of an object relative to face of a camera sensor . I need to measure the following

1. Distance camera sensor to object ( Must be between 3-4cm)
2. Object must be parallel to face of camera sensor ( the camera sensor is not static , it is being held by an individual )

I'm thinking best solution may be ZX Distance and Gesture Sensor, however I'm not sure this will give me "if parallel" answer

Any help in a possible solution would be grateful

Thanks
By jremington
#199026
Describe object.

For an arbitrary object, how do you define "parallel to face of camera sensor"?
By tonyr
#199029
The object is a palm of a hand.

I guess Im looking for a device/ sensor that measures angle that object is relative to sensor device , to an

I know there are many sensors that will provide distance to an object , I'm looking for a sensor to return the angle object is to measuring sensor

In my case, the object is the palm of a hand

Hope this helps and thanks for response
By jremington
#199030
Assuming that the palm is held flat, two or more distance measurements and some geometry can be used to determine the angles involved.

Non-scanning distance sensors return only one measurement at a time, so you would have to use several pointing in different directions, or figure out how to aim one.