- Tue May 09, 2017 1:40 am
#194760
Hello all,
I was wondering if someone tried running Pro Micro using 11.1v 3S Lipo via RAW pin. The reason why I am asking is because when fully charged 3S LIPO battery has approx 12.6 volts which is above 12V for powering over RAW pin according to documentation. The board itself will be controlling motor connected to same LIPO battery via MOSFET by supplying 5V voltage to the gate from one of the PWM capable pins.
Thanks in advance.
I was wondering if someone tried running Pro Micro using 11.1v 3S Lipo via RAW pin. The reason why I am asking is because when fully charged 3S LIPO battery has approx 12.6 volts which is above 12V for powering over RAW pin according to documentation. The board itself will be controlling motor connected to same LIPO battery via MOSFET by supplying 5V voltage to the gate from one of the PWM capable pins.
Thanks in advance.