- Sun Apr 16, 2017 2:03 pm
#194396
Hello, I am a newbie to ardunio. I built an alarm system using PIR sensor, LED bulb, Ardunio Uno and Adafruit CC3000 Wifi Shield and now i am having some problems. I have also built an android mobile application to this project
First the LED bulb lights up slightly when motion is detected.
I have created a code which send notifications to my android application when motion is detected. but i dont receive notifications when the pir sensor detects motion. but the android application receives a notification when i upload the code to the Ardunio Uno board. I have no idea where the problem is or how to correct it.
I dont know how to edit this code. What should i Do?
Yuuki
First the LED bulb lights up slightly when motion is detected.
I have created a code which send notifications to my android application when motion is detected. but i dont receive notifications when the pir sensor detects motion. but the android application receives a notification when i upload the code to the Ardunio Uno board. I have no idea where the problem is or how to correct it.
Code: Select all
I have used the Webclient example in the ardunio.I need to build my code such that it send a true message to the given website when the sensor detects motion.#include <Adafruit_CC3000.h>
#include <ccspi.h>
#include <SPI.h>
#include <string.h>
#include "utility/debug.h"
// These are the interrupt and control pins
#define ADAFRUIT_CC3000_IRQ 3 // MUST be an interrupt pin!
// These can be any two pins
#define ADAFRUIT_CC3000_VBAT 5
#define ADAFRUIT_CC3000_CS 10
// Use hardware SPI for the remaining pins
// On an UNO, SCK = 13, MISO = 12, and MOSI = 11
Adafruit_CC3000 cc3000 = Adafruit_CC3000(ADAFRUIT_CC3000_CS, ADAFRUIT_CC3000_IRQ, ADAFRUIT_CC3000_VBAT,
SPI_CLOCK_DIVIDER); // you can change this clock speed
#define WLAN_SSID "dlink_DWR-730_1A31" // cannot be longer than 32 characters!
#define WLAN_PASS "hAMpU34443"
// Security can be WLAN_SEC_UNSEC, WLAN_SEC_WEP, WLAN_SEC_WPA or WLAN_SEC_WPA2
#define WLAN_SECURITY WLAN_SEC_WPA2
#define IDLE_TIMEOUT_MS 3000 // Amount of time to wait (in milliseconds) with no data
// received before closing the connection. If you know the server
// you're accessing is quick to respond, you can reduce this value.
// What page to grab!
#define WEBSITE "www.m-register.com"
#define WEBPAGE "/urlval.php?status=true"
int sensor=7;
int push_switch=2;
int buzzer=8;
int sensor_value;
uint32_t ip;
void setup(void)
{
Serial.begin(9600);
Serial.println(F("Hello, CC3000!\n"));
Serial.print("Free RAM: "); Serial.println(getFreeRam(), DEC);
/* Initialise the module */
Serial.println(F("\nInitializing..."));
if (!cc3000.begin())
{
Serial.println(F("Couldn't begin()! Check your wiring?"));
while(1);
}
// Optional SSID scan
// listSSIDResults();
Serial.print(F("\nAttempting to connect to ")); Serial.println(WLAN_SSID);
if (!cc3000.connectToAP(WLAN_SSID, WLAN_PASS, WLAN_SECURITY)) {
Serial.println(F("Failed!"));
while(1);
}
Serial.println(F("Connected!"));
/* Wait for DHCP to complete */
Serial.println(F("Request DHCP"));
while (!cc3000.checkDHCP())
{
delay(100); // ToDo: Insert a DHCP timeout!
}
/* Display the IP address DNS, Gateway, etc. */
while (! displayConnectionDetails()) {
delay(1000);
}
ip = 0;
// Try looking up the website's IP address
Serial.print(WEBSITE); Serial.print(F(" -> "));
while (ip == 0) {
if (! cc3000.getHostByName(WEBSITE, &ip)) {
Serial.println(F("Couldn't resolve!"));
}
delay(500);
}
cc3000.printIPdotsRev(ip);
// Optional: Do a ping test on the website
/*
Serial.print(F("\n\rPinging ")); cc3000.printIPdotsRev(ip); Serial.print("...");
replies = cc3000.ping(ip, 5);
Serial.print(replies); Serial.println(F(" replies"));
*/
/* Try connecting to the website.
Note: HTTP/1.1 protocol is used to keep the server from closing the connection before all data is read.
*/
Adafruit_CC3000_Client www = cc3000.connectTCP(ip, 80);
if (www.connected()) {
www.fastrprint(F("GET "));
www.fastrprint(WEBPAGE);
www.fastrprint(F(" HTTP/1.1\r\n"));
www.fastrprint(F("Host: ")); www.fastrprint(WEBSITE);www.fastrprint(F("\r\n"));
www.fastrprint(F("\r\n"));
www.println();
} else {
Serial.println(F("Connection failed"));
return;
}
Serial.println(F("-------------------------------------"));
/* Read data until either the connection is closed, or the idle timeout is reached. */
unsigned long lastRead = millis();
while (www.connected() && (millis() - lastRead < IDLE_TIMEOUT_MS)) {
while (www.available()) {
char c = www.read();
Serial.print(c);
lastRead = millis();
}
}
www.close();
Serial.println(F("-------------------------------------"));
/* You need to make sure to clean up after yourself or the CC3000 can freak out */
/* the next time your try to connect ... */
Serial.println(F("\n\nDisconnecting"));
cc3000.disconnect();
}
void loop(void)
{ sensor_value=digitalRead(sensor);
//Serial.println(sensor_value);
if(sensor_value==HIGH)
{
digitalWrite(buzzer,HIGH);
}
if(digitalRead(push_switch==HIGH))
{
digitalWrite(buzzer,LOW);
}
delay(1000);
}
/**************************************************************************/
/*!
@brief Begins an SSID scan and prints out all the visible networks
*/
/**************************************************************************/
void listSSIDResults(void)
{
uint32_t index;
uint8_t valid, rssi, sec;
char ssidname[33];
if (!cc3000.startSSIDscan(&index)) {
Serial.println(F("SSID scan failed!"));
return;
}
Serial.print(F("Networks found: ")); Serial.println(index);
Serial.println(F("================================================"));
while (index) {
index--;
valid = cc3000.getNextSSID(&rssi, &sec, ssidname);
Serial.print(F("SSID Name : ")); Serial.print(ssidname);
Serial.println();
Serial.print(F("RSSI : "));
Serial.println(rssi);
Serial.print(F("Security Mode: "));
Serial.println(sec);
Serial.println();
}
Serial.println(F("================================================"));
cc3000.stopSSIDscan();
}
/**************************************************************************/
/*!
@brief Tries to read the IP address and other connection details
*/
/**************************************************************************/
bool displayConnectionDetails(void)
{
uint32_t ipAddress, netmask, gateway, dhcpserv, dnsserv;
if(!cc3000.getIPAddress(&ipAddress, &netmask, &gateway, &dhcpserv, &dnsserv))
{
Serial.println(F("Unable to retrieve the IP Address!\r\n"));
return false;
}
else
{
Serial.print(F("\nIP Addr: ")); cc3000.printIPdotsRev(ipAddress);
Serial.print(F("\nNetmask: ")); cc3000.printIPdotsRev(netmask);
Serial.print(F("\nGateway: ")); cc3000.printIPdotsRev(gateway);
Serial.print(F("\nDHCPsrv: ")); cc3000.printIPdotsRev(dhcpserv);
Serial.print(F("\nDNSserv: ")); cc3000.printIPdotsRev(dnsserv);
Serial.println();
return true;
}}
I dont know how to edit this code. What should i Do?
Yuuki