- Sat Oct 29, 2016 5:08 pm
#192229
Hello,
I am working on a robotic system that uses four different stepper motors. Because of the different current ratings of the motors, I have one running on a L293N driver board, one on an EasyDriver, one on a Big EasyDriver, and the last one on an Autodriver v10. When I run my code using only the three non-AutoDriver steppers, each one works as expected. However, when I include the line that runs the AutoDriver, all of the motors stop, only jittering occasionally.
I have the AutoDriver configured in setup(), so could this be an issue with the SPI connection or chip select? (I'm using an Arduino Mega 2560.) What might be causing all the other motors to stop running?
I am working on a robotic system that uses four different stepper motors. Because of the different current ratings of the motors, I have one running on a L293N driver board, one on an EasyDriver, one on a Big EasyDriver, and the last one on an Autodriver v10. When I run my code using only the three non-AutoDriver steppers, each one works as expected. However, when I include the line that runs the AutoDriver, all of the motors stop, only jittering occasionally.
I have the AutoDriver configured in setup(), so could this be an issue with the SPI connection or chip select? (I'm using an Arduino Mega 2560.) What might be causing all the other motors to stop running?