- Wed Aug 03, 2016 5:45 pm
#190986
I've searched around and haven't been able to find help so hopefully this forum can help. I've compiled the latest OpenOCD (Open On-Chip Debugger 0.10.0-dev-00330-g5d5c9bc) and am running it on a Raspberry Pi. My openocd.cfg file has the following in it:
This is my first time using OpenOCD so I wouldn't be surprised if I've missed something. When I start the session I get the following:
Thanks in advance for anyone's help,
George
Code: Select all
My end goal is to try and program a Proc BLE part but before I tried that I thought it best to try a CY8CKIT-049-41xx PSoC 4 Prototyping kit since I thought this board was supported.source [find interface/raspberrypi2-native.cfg]
transport select swd
set CHIPNAME at91samd21g18
#source [find target/at91samdXX.cfg]
source [find target/psoc4.cfg]
# did not yet manage to make a working setup using srst
#reset_config srst_only
reset_config srst_nogate
adapter_nsrst_delay 100
adapter_nsrst_assert_width 100
init
targets
reset halt
This is my first time using OpenOCD so I wouldn't be surprised if I've missed something. When I start the session I get the following:
Code: Select all
If I comment out line 17 (reset halt). I get this:
pi@raspberrypi:~/cypress $ sudo openocd
Open On-Chip Debugger 0.10.0-dev-00330-g5d5c9bc (2016-08-03-13:52)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
BCM2835 GPIO nums: swclk = 25, swdio = 24
BCM2835 GPIO config: srst = 18
srst_only separate srst_gates_jtag srst_push_pull connect_deassert_srst
adapter speed: 1500 kHz
cortex_m reset_config sysresetreq
srst_only separate srst_nogate srst_push_pull connect_deassert_srst
adapter_nsrst_delay: 100
adapter_nsrst_assert_width: 100
Info : BCM2835 GPIO JTAG/SWD bitbang driver
Info : SWD only mode enabled (specify tck, tms, tdi and tdo gpios to add JTAG mode)
Info : clock speed 1507 kHz
Info : SWD DPIDR 0x0bb11477
Info : at91samd21g18.cpu: hardware has 4 breakpoints, 2 watchpoints
TargetName Type Endian TapName State
-- ------------------ ---------- ------ ------------------ ------------
0* at91samd21g18.cpu cortex_m little at91samd21g18.cpu running
PSoC 4 reset can handle only one psoc4.cpu target
in procedure 'reset' called at file "openocd.cfg", line 17
in procedure 'ocd_bouncer'
Code: Select all
So I'm stuck with it unable to initialize the debug port. I've checked the obvious things like wiring and everything seems OK so I'll have to assume it's something with the configuration.pi@raspberrypi:~/cypress $ sudo openocd
Open On-Chip Debugger 0.10.0-dev-00330-g5d5c9bc (2016-08-03-13:52)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
BCM2835 GPIO nums: swclk = 25, swdio = 24
BCM2835 GPIO config: srst = 18
srst_only separate srst_gates_jtag srst_push_pull connect_deassert_srst
adapter speed: 1500 kHz
cortex_m reset_config sysresetreq
srst_only separate srst_nogate srst_push_pull connect_deassert_srst
adapter_nsrst_delay: 100
adapter_nsrst_assert_width: 100
Info : BCM2835 GPIO JTAG/SWD bitbang driver
Info : SWD only mode enabled (specify tck, tms, tdi and tdo gpios to add JTAG mode)
Info : clock speed 1507 kHz
Info : SWD DPIDR 0x0013d9a8
Error: Could not initialize the debug port
TargetName Type Endian TapName State
-- ------------------ ---------- ------ ------------------ ------------
0* at91samd21g18.cpu cortex_m little at91samd21g18.cpu unknown
Thanks in advance for anyone's help,
George