- Sun Nov 22, 2015 5:53 am
#186082
I have a new SparkFun SAMD21 Dev Breakout board. Compile/Upload is where I have a problem.
It takes a long time for even the smallest of programs. The text below is the compile/upload of the blink program.
I don't understand why this is so much different than the other arduino boards I use. Am I doing something wrong?
The text below is the output window in the arduino ide..
Thanks in advance,
Jim
It takes a long time for even the smallest of programs. The text below is the compile/upload of the blink program.
I don't understand why this is so much different than the other arduino boards I use. Am I doing something wrong?
The text below is the output window in the arduino ide..
Thanks in advance,
Jim
Warning: platform.txt from core 'Arduino SAMD (32-bits ARM Cortex-M0+) Boards' contains deprecated recipe.ar.pattern="{compiler.path}{compiler.ar.cmd}" {compiler.ar.flags} {compiler.ar.extra_flags} "{build.path}/{archive_file}" "{object_file}", automatically converted to recipe.ar.pattern="{compiler.path}{compiler.ar.cmd}" {compiler.ar.flags} {compiler.ar.extra_flags} "{archive_file_path}" "{object_file}". Consider upgrading this core.
Warning: platform.txt from core 'SparkFun SAMD (32-bits ARM Cortex-M0+) Boards' contains deprecated recipe.ar.pattern="{compiler.path}{compiler.ar.cmd}" {compiler.ar.flags} {compiler.ar.extra_flags} "{build.path}/{archive_file}" "{object_file}", automatically converted to recipe.ar.pattern="{compiler.path}{compiler.ar.cmd}" {compiler.ar.flags} {compiler.ar.extra_flags} "{archive_file_path}" "{object_file}". Consider upgrading this core.
Sketch uses 11,596 bytes (4%) of program storage space. Maximum is 262,144 bytes.
Atmel SMART device 0x10010005 found
Device : ATSAMD21G18A
Chip ID : 10010005
Version : v1.1 [SparkFun:XYZ] Sep 24 2015 16:50:58
Address : 8192
Pages : 3968
Page Size : 64 bytes
Total Size : 248KB
Planes : 1
Lock Regions : 16
Locked : none
Security : false
Boot Flash : true
BOD : true
BOR : true
Erase flash
done in 46.441 seconds
Write 11772 bytes to flash (184 pages)
[ ] 0% (0/184 pages)
[== ] 9% (18/184 pages)
[===== ] 19% (36/184 pages)
[======== ] 29% (54/184 pages)
[=========== ] 39% (72/184 pages)
[============== ] 48% (90/184 pages)
[================= ] 58% (108/184 pages)
[==================== ] 68% (126/184 pages)
[======================= ] 78% (144/184 pages)
[========================== ] 88% (162/184 pages)
[============================= ] 97% (180/184 pages)
[==============================] 100% (184/184 pages)
done in 28.704 seconds
Verify 11772 bytes of flash
[ ] 0% (0/184 pages)
[== ] 9% (18/184 pages)
[===== ] 19% (36/184 pages)
[======== ] 29% (54/184 pages)
[=========== ] 39% (72/184 pages)
[============== ] 48% (90/184 pages)
[================= ] 58% (108/184 pages)
[==================== ] 68% (126/184 pages)
[======================= ] 78% (144/184 pages)
[========================== ] 88% (162/184 pages)
[============================= ] 97% (180/184 pages)
[==============================] 100% (184/184 pages)
Verify successful
done in 0.203 seconds
CPU reset.