- Sun Jun 21, 2015 9:46 am
#182815
I am willing to use most any platform! I have 8 sensors that I currently have preconditioned through an existing differential, variable gain, non-programmable board. My output is 8 high level, single ended, analog. I would like to mux and digitize within a foot or so of the preamp and supply a serial stream to a location about 40 feet away, taking the curvy route. I have a Sabrent serial/usb adapter cable at my disposal. At the remote location I would like to use a piece of compatible software so that I can do data logging or some realtime observation. In my favor, the speed of the system can be quite slow, with only a couple of conversions per channel per second being needed. I could live with even a magnitude less than that.
Back at the a/d converter, a single supply of +12v would be best, but I will entertain a dc/dc converter if necessary. Resolution is good at 12 bits, will consider 10 bits if i must. I do not have need for a case, but location for standoffs would be necessary. I would appreciate easy termination for i/o. Because of distance between the a/d and the monitor location, usb is out, rf is in, so is rs-232. A baud rate 0f 4800 will more than cover my cps requirements. I am looking for a small (whatever that means) footprint, but I can stack vertically. The monitor computer uses linux as the os, but I do use virtualbox and have ms xp installed. I may be able to come up with other ms os's as well, if forced to.
I do not have much time available for programming so a functional, compatible software, integrating all components is very desirable.
And, of course, inexpensive wins.
What do you recommend?
Back at the a/d converter, a single supply of +12v would be best, but I will entertain a dc/dc converter if necessary. Resolution is good at 12 bits, will consider 10 bits if i must. I do not have need for a case, but location for standoffs would be necessary. I would appreciate easy termination for i/o. Because of distance between the a/d and the monitor location, usb is out, rf is in, so is rs-232. A baud rate 0f 4800 will more than cover my cps requirements. I am looking for a small (whatever that means) footprint, but I can stack vertically. The monitor computer uses linux as the os, but I do use virtualbox and have ms xp installed. I may be able to come up with other ms os's as well, if forced to.
I do not have much time available for programming so a functional, compatible software, integrating all components is very desirable.
And, of course, inexpensive wins.
What do you recommend?