- Thu Jun 11, 2015 8:43 pm
#182635
I am trying to get 28F640J3 CFI external NOR flash interface to ks8695 (ARM922T core) show up in openocd. I am using Segger Jlink JTAG interface.
The flash banks are arranged in the 2 banks with 4 chips, each 64Mbit 8Mx8 which makes each chip 8MByte or total 8MByte x 4 = 32 MBytes, as shown in the image (hopefully the image url won't go down anytime soon!). The comment on the file below though states 'Each bank is 16-bits wide, two 16-bit chips in parallel'. It also has 32 MB SDRAM.
From the datasheet System configuration registers I found
0x3ff4000-0x3ff4040 are of our interest. I luckily found something for the board in archives which I thought would be of our interest
I am wondering why bank 0 cannot be found while seemingly bank 1 is found? Also I suspect my settings for NOR registers may be incorrect or may need some more tweaking. Any help is appreciated.
The flash banks are arranged in the 2 banks with 4 chips, each 64Mbit 8Mx8 which makes each chip 8MByte or total 8MByte x 4 = 32 MBytes, as shown in the image (hopefully the image url won't go down anytime soon!). The comment on the file below though states 'Each bank is 16-bits wide, two 16-bit chips in parallel'. It also has 32 MB SDRAM.
From the datasheet System configuration registers I found
0x3ff4000-0x3ff4040 are of our interest. I luckily found something for the board in archives which I thought would be of our interest
Code: Select all
Based on this file I tried to write openocd file as follows and tweak 0x3ff4010,0x3ff4014 and 0x3ff4014 to get this CFI FLASH to recognized. After I tweaked 0x3ff4014 looking at the datasheet my bank 1 CFI would show up as two separate CFI chips since I used 4 'flash bank ....' commands because even though I have 2 banks - there are 4 chips 8 MByte each. I am not sure if my config below is correct. The start address for flash bank 0 is 0x02000000 and similarly for flash bank 1 is 0x03000000. When I run //comment this is the board init configuration file
//comment which sets up the sdram and flash memory
//comment so that user can download code into sdram
//comment and run it.
//comment This file is used to enabe the demo board
//comment when there is no code resides in the flash
//comment memory.
//comment set up external banks
//DEVICE ALE
//B31:22 = 3FC (end address = 0x3FCFFFF)
//B21:12 = 3FC (start address = 0x3FC0000)
dword(0x03FF4000) = 0xFF3FCFFF
//DEVICE RD
//B31:22 = 3FD (end address = 0x3FDFFFF)
//B21:12 = 3FD (start address = 0x3FD0000)
dword(0x03FF4004) = 0xFF7FDFFF
//DEVICE WR
//B31:22 = 3FE (end address = 0x3FEFFFF)
//B21:12 = 3FE (start address = 0x3FE0000)
dword(0x03FF4008) = 0xFFBFEFFF
// *** Set up rom/flash ***
//Bank 0
//B31:22 = 2FF (end address = 0x2FFFFFF)
//B21:12 = 200 (start address = 0x2000000)
dword(0x03FF4010) = 0xBFE00070
//Bank 1
//B31:22 = 3FB (end address = 0x3FBFFFF)
//B21:12 = 300 (start address = 0x3000000)
dword(0x03FF4014) = 0xFEF00070
//External I/O and ROM/SRAM/FLASH General Register
// Enable CAN RD, CAN WR and CAN ALE
dword(0x03FF4020) = 0x30FF000F
// *** Set up SDRAM ***
//SDRAM Control Register 0 (0x4030)
//B31:22 = 0FF (end address = 0xFFFFFF)
//B21:12 = 000 (start address = 0x0)
dword(0x03FF4030) = 0x3FC0000E
//SDRAM Control Register 1 (0x4034)
//B31:22 = 1FF (end address = 0x1FFFFFF)
//B21:12 = 100 (start address = 0x1000000)
dword(0x03FF4034) = 0x7FD0000E
dword(0x03FF4038) = 0x0000000A
//comment send NOP command
dword(0x03FF403C) = 0x00030000
//comment wait for command to complete
//comment send precharge command
dword(0x03FF403C) = 0x00010000
//comment wait for command to complete
dword(0x03FF4040) = 0x00000014
//comment wait for command to complete
//comment set the refresh timer back
dword(0x03FF4040) = 0x00000168
//comment wait for command to complete
//comment send Mode command
dword(0x03FF403C) = 0x00020033 //0x00020003
//comment set clock to be the fastest one
dword(0x03FF0004) = 0x00
//comment memory configured.
Code: Select all
$: openocd -f enthusiasticgeek.cfg
#and in another window
$: telnet 127.0.0.1 4444
> reset init
> reset init; flash probe 0; flash probe 1 #<--------------Seems like it finds chip but unable to communicate with CFI driver :( :doh:
... reset-start ....
adapter speed: 8 kHz
JTAG tap: ks869x.cpu tap/device found: 0x00922f0f (mfg: 0x787, part: 0x0922, ver: 0x0)
... reset-assert ....
srst pulls trst - can not reset into halted mode. Issuing halt after reset.
target state: halted
target halted in ARM state due to debug-request, current mode: System
cpsr: 0xe00000df pc: 0x00000038
MMU: disabled, D-Cache: disabled, I-Cache: disabled
... reset-init ....
... Executing procedure acs5k_init_load_code_into_sdram....
... init routine ...
adapter speed: 8000 kHz
dcc downloads are enabled
NOTE! Severe performance degradation without fast memory access enabled. Type 'help fast'.
Flash Manufacturer/Device: 0xf0d7 0x0089
Could not probe bank: no QRY
Try workaround w/0x555 instead of 0x55 to get QRY.
Could not probe bank: no QRY
auto_probe failed
in procedure 'flash'
> reset init; flash probe 2; flash probe 3 #<------------------------------------------------------ Seems to WORK!!! :dance:
... reset-start ....
adapter speed: 8 kHz
JTAG tap: ks869x.cpu tap/device found: 0x00922f0f (mfg: 0x787, part: 0x0922, ver: 0x0)
... reset-assert ....
srst pulls trst - can not reset into halted mode. Issuing halt after reset.
target state: halted
target halted in ARM state due to debug-request, current mode: System
cpsr: 0xe00000df pc: 0x0000002c
MMU: disabled, D-Cache: disabled, I-Cache: disabled
... reset-init ....
... Executing procedure acs5k_init_load_code_into_sdram....
... init routine ...
adapter speed: 8000 kHz
dcc downloads are enabled
NOTE! Severe performance degradation without fast memory access enabled. Type 'help fast'.
Flash Manufacturer/Device: 0x0089 0x0017
Flash Manufacturer/Device: 0x0089 0x0017
flash 'cfi' found at 0x03000000
Flash Manufacturer/Device: 0x0089 0x0017
Flash Manufacturer/Device: 0x0089 0x0017
flash 'cfi' found at 0x03800000
Code: Select all
#File: enthusiasticgeek.cfg
#Config file Author: enthusiasticgeek
#June 2015
#To test the JTAG connection to the board one can simply run the
#openocd -f /usr/local/share/openocd/scripts/interface/jlink.cfg -c "gdb_memory_map enable" -c "gdb_flash_program enable" -f /usr/local/share/openocd/scripts/target/ks869x.cfg
source [find interface/jlink.cfg]
#GDB can also flash my flash!
gdb_memory_map enable
gdb_flash_program enable
# ARM920T CPU
if { [info exists CHIPNAME] } {
set _CHIPNAME $CHIPNAME
} else {
set _CHIPNAME ks869x
}
if { [info exists ENDIAN] } {
set _ENDIAN $ENDIAN
} else {
set _ENDIAN little
}
if { [info exists CPUTAPID] } {
set _CPUTAPID $CPUTAPID
} else {
set _CPUTAPID 0x00922f0f
}
if { [info exists FLASHTAPID] } {
set _FLASHTAPID $FLASHTAPID
} else {
set _FLASHTAPID 0x890017
}
debug_level 3
# telnet and gdb_ports
telnet_port 4444
gdb_port 3333
reset_config trst_and_srst srst_pulls_trst
# set adapter_nsrst_delay to the delay introduced by your reset circuit
# the rest of the needed delays are built into the openocd program
adapter_nsrst_delay 260
# set the jtag_ntrst_delay to the delay introduced by a reset circuit
# the rest of the needed delays are built into the openocd program
jtag_ntrst_delay 250
adapter_khz 4
# jtag scan chain
# Add new test access port
jtag newtap $_CHIPNAME cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id $_CPUTAPID
#set CPU target name
set _TARGETNAME $_CHIPNAME.cpu
target create $_TARGETNAME arm920t -endian $_ENDIAN -chain-position $_TARGETNAME
#-variant arm922t
#Internal SRAM work area (typically equivalent L1,L2,L3 caches in x86)
$_TARGETNAME configure -work-area-phys 0x20000 -work-area-size 0x20000 -work-area-backup 0
# speed up memory downloads
arm7_9 fast_memory_access enable
arm7_9 dcc_downloads enable
#foreach t [jtag names] {
# puts [format " ======= TAP Found: %s =======\n" $t]
#}
$_TARGETNAME configure -event "reset-assert" {
echo "... reset-assert ...."
#cortex_a dbginit
}
$_TARGETNAME configure -event "reset-start" {
echo "... reset-start ...."
adapter_khz 8
}
$_TARGETNAME configure -event "reset-init" {
echo "... reset-init ...."
echo "... Executing procedure _init_load_code_into_sdram...."
_init_load_code_into_sdram
}
#####################
# CFI Flash configuration
#####################
# flash bank <driver> <base> <size> <chip_width> <bus_width>
# CS0, CS1 -- two banks of CFI flash, 16 MBytes each
# each bank is 16-bits wide, two 16-bit chips in parallel
set _FLASHNAME $_CHIPNAME.flash0
flash bank $_FLASHNAME cfi 0x02000000 0x0800000 2 2 $_TARGETNAME
set _FLASHNAME $_CHIPNAME.flash1
flash bank $_FLASHNAME cfi 0x02800000 0x0800000 2 2 $_TARGETNAME
set _FLASHNAME $_CHIPNAME.flash2
flash bank $_FLASHNAME cfi 0x03000000 0x0800000 2 2 $_TARGETNAME
set _FLASHNAME $_CHIPNAME.flash3
flash bank $_FLASHNAME cfi 0x03800000 0x0800000 2 2 $_TARGETNAME
init
proc _init_load_code_into_sdram { } {
echo "... init routine ..."
#this is the board init configuration file
#which sets up the sdram and flash memory
#so that user can download code into sdram
#and run it.
#This file is used to enabe the demo board
#when there is no code resides in the flash
#memory
adapter_khz 8000
arm7_9 dcc_downloads enable ;# Enable faster DCC downloads
#Time to set up the SDRAM and Flash memory
#comment set up external banks
#CAN ALE
#B31:22 = 3FC (end address = 0x3FCFFFF)
#B21:12 = 3FC (start address = 0x3FC0000)
#dword(0x03FF4000) = 0xFF3FCFFF
mww 0x03ff4000 0xff3fcfff
#CAN RD
#B31:22 = 3FD (end address = 0x3FDFFFF)
#B21:12 = 3FD (start address = 0x3FD0000)
#dword(0x03FF4004) = 0xFF7FDFFF
mww 0x03ff4004 0xff7fdfff
#CAN WR
#B31:22 = 3FE (end address = 0x3FEFFFF)
#B21:12 = 3FE (start address = 0x3FE0000)
#dword(0x03FF4008) = 0xFFBFEFFF
mww 0x03ff4008 0xffbfefff
#======================================================================
#################### MOST IMPORTANT TO BURN IMAGE #####################
#======================================================================
# *** Set up rom/flash ***
#======================================================================
#Bank 0
#B31:22 = 2FF (end address = 0x2FFFFFF)
#B21:12 = 200 (start address = 0x2000000)
#dword(0x03FF4010) = 0xBFE00070
mww 0x03ff4010 0xbfe00070
#Bank 1
#B31:22 = 3FB (end address = 0x3FBFFFF)
#B21:12 = 300 (start address = 0x3000000)
#dword(0x03FF4014) = 0xFEF00070
mww 0x03ff4014 0xfef00070
#External I/O and ROM/SRAM/FLASH General Register
# Enable CAN RD, CAN WR and CAN ALE
#dword(0x03FF4020) = 0x30FF000F
#mww 0x03ff4020 0x30ff000f
mww 0x03ff4020 0x30ff000a
#======================================================================
#======================================================================
# *** Set up SDRAM ***
#======================================================================
#SDRAM Control Register 0 (0x4030)
#B31:22 = 0FF (end address = 0xFFFFFF)
#B21:12 = 000 (start address = 0x0)
#dword(0x03FF4030) = 0x3FC0000E
mww 0x03ff4030 0x3fc0000e
#SDRAM Control Register 1 (0x4034)
#B31:22 = 1FF (end address = 0x1FFFFFF)
#B21:12 = 100 (start address = 0x1000000)
#dword(0x03FF4034) = 0x7FD0000E
mww 0x03ff4034 0x7fd0000e
# Set global RAS/CAS timing
#dword(0x03FF4038) = 0x0000000A
mww 0x03ff4038 0x0000000a
#======================================================================
#comment send NOP command
#dword(0x03FF403C) = 0x00030000
mww 0x03ff403c 0x00030000
#comment wait for command to complete
#comment send precharge command
#dword(0x03FF403C) = 0x00010000
mww 0x03ff403c 0x00010000
#comment wait for command to complete
#dword(0x03FF4040) = 0x00000014
mww 0x03ff4040 0x00000014
#comment wait for command to complete
#comment set the refresh timer back
#dword(0x03FF4040) = 0x00000168
mww 0x03ff4040 0x00000168
#comment wait for command to complete
#comment send Mode command
#dword(0x03FF403C) = 0x00020033 #0x00020003
mww 0x03ff403c 0x00020033
#comment set clock to be the fastest one
#dword(0x03FF0004) = 0x00
mww 0x03ff4004 0x00000000
halt
#flash probe 0 ;# Identify flash bank 0
}
#Important URLs
#http:#translate.google.com/translate?hl=en&sl=ja&u=http:#sonare.jp/wiki/%3FBLR-TX4M&prev=search
#https:#github.com/rhuitl/uClinux/blob/master/tools/misc/sg310.gdb
I am wondering why bank 0 cannot be found while seemingly bank 1 is found? Also I suspect my settings for NOR registers may be incorrect or may need some more tweaking. Any help is appreciated.