- Wed May 27, 2015 3:50 pm
#182291
I have a Pro Micro board..
I realized that the SS pin on the SPI bus is NOT broken out to any I/O pins for us to use...
I find it odd that a board would be released that wont support any SPI devices?.. So there must be a way around this... no?
How can you define or use a different pin as the SS pin when using a Pro Micro as the base?
(for full disclosure, I want to use this with the USB Host Mini Shield from Circuits @ Home)
The (mini) shield was designed to be used with a Pro Mini...
The Pro Micro is basically a Leonardo, in the same footprint/size of the Pro Mini...(with the exception of the RESET pin is not in the same location.. not sure why this done?).. and the SPI bus is only partially broken out to the I/O pins
MOSI - 16
MISO - 14
SCLK - 15
SS pin is pin#17, but is not broken out.. and is hardcoded to the RX, yellow on-board led?
How do you overcome this?
Can you delcare/set pin #17 as an output.. or enable internal pull-up resistor?.. and then (somewhere) re-define the SS pin? (in the USB Host library I'm guessing this step)
Circuits @ Home says.. they are not familiar with the Pro Micro, so have not been any help.
I figured, I need to come to the source then.
Thanks!
-xl
I realized that the SS pin on the SPI bus is NOT broken out to any I/O pins for us to use...
I find it odd that a board would be released that wont support any SPI devices?.. So there must be a way around this... no?
How can you define or use a different pin as the SS pin when using a Pro Micro as the base?
(for full disclosure, I want to use this with the USB Host Mini Shield from Circuits @ Home)
The (mini) shield was designed to be used with a Pro Mini...
The Pro Micro is basically a Leonardo, in the same footprint/size of the Pro Mini...(with the exception of the RESET pin is not in the same location.. not sure why this done?).. and the SPI bus is only partially broken out to the I/O pins
MOSI - 16
MISO - 14
SCLK - 15
SS pin is pin#17, but is not broken out.. and is hardcoded to the RX, yellow on-board led?
How do you overcome this?
Can you delcare/set pin #17 as an output.. or enable internal pull-up resistor?.. and then (somewhere) re-define the SS pin? (in the USB Host library I'm guessing this step)
Circuits @ Home says.. they are not familiar with the Pro Micro, so have not been any help.
I figured, I need to come to the source then.
Thanks!
-xl