- Thu Feb 26, 2015 7:33 am
#180068
Hi...I have the edison with the spark fun starter blocks as well as the I2C block. I have them all stacked and the edison is working fine, but I'm having issues with the I2C block. I'm trying to use it with the HTU21D temperature and humidity sensor, but once connected I dont see it via i2cdetect and I get what I assume are default values back when I try to run the code sample for the HTU21D on the edison ('Time:506220 Temperature:998.0C Humidity:998.0%'). The sensor is I2C and it does run at 3.3V, so I assumed it would be fine. I'll keep playing around, but wanted to make sure I wasnt missing something.