- Thu Feb 12, 2015 7:51 pm
#179687
Hi,
i have the AutoDriver board connected to an UNO R3 and a NEMA17 stepper. The dSPIN example from the library works fine so i know my hardware and connections are in good order. However, the AutoDriver example doesn't move the motor. The sketch does run and interacts with the serial monitor (accepting user input, printing text as programmed), however there is no action on the motor. Is there a different setup i need to have for the AutoDriver example to work? Or are there known issues with the AutoDriver example? Any advice is appreciated. I even tried commenting out all the references to boardB, same result unfortunately.
Thanks,
Chip
i have the AutoDriver board connected to an UNO R3 and a NEMA17 stepper. The dSPIN example from the library works fine so i know my hardware and connections are in good order. However, the AutoDriver example doesn't move the motor. The sketch does run and interacts with the serial monitor (accepting user input, printing text as programmed), however there is no action on the motor. Is there a different setup i need to have for the AutoDriver example to work? Or are there known issues with the AutoDriver example? Any advice is appreciated. I even tried commenting out all the references to boardB, same result unfortunately.
Thanks,
Chip