- Fri Dec 12, 2014 9:13 am
#177638
Hello,
How does the power select work on the Arduino Pro Mini 3.3V/8MHz? In other words, if I connect both a RAW input (a 7.4V battery for my system) and FTDI VCC input (3.3V programming header input), what will the mini run off? I ask because my system only works when both these power sources are connected at the same time, i.e. when the battery is plugged into RAW and the programming headers are plugged in (in order to program on-the-fly and communicate through UART).
Additional background/clarification: My system consists of the arduino pro mini and a drv8833 carrier board, a 7.4V LiPo, and two motors. When powered from from the LiPo, my motors spasm/lock/stall. Motors work normally when Arduino pro mini board receives power from 3.3V VCC programming header pin and 7.4V RAW battery input.
How does the power select work on the Arduino Pro Mini 3.3V/8MHz? In other words, if I connect both a RAW input (a 7.4V battery for my system) and FTDI VCC input (3.3V programming header input), what will the mini run off? I ask because my system only works when both these power sources are connected at the same time, i.e. when the battery is plugged into RAW and the programming headers are plugged in (in order to program on-the-fly and communicate through UART).
Additional background/clarification: My system consists of the arduino pro mini and a drv8833 carrier board, a 7.4V LiPo, and two motors. When powered from from the LiPo, my motors spasm/lock/stall. Motors work normally when Arduino pro mini board receives power from 3.3V VCC programming header pin and 7.4V RAW battery input.