- Thu Aug 21, 2014 10:11 am
#173946
Hi guys,
I just bought the Bluetooth Mate Silver so I could wire it to my Arduino Uno R3. My final purpose is to connect Arduino to my phone via BT.
I followed the tutorial for the BT modules to hook it up with Arduino, but I can't get past the first example sketches.
when I try the basic sketch, or the passthrough sketch, my code never returns true on bluetooth.available(). So I can't communicate with the bluetooth mate.
I've tried playing with the baudrates, changing Arduino IDE versions and computer settings & OS (Win 7 & Linux). But still no results.
Can anyone guide me towards a solution? Thanks in advance...
This is de sketch I am using:
I just bought the Bluetooth Mate Silver so I could wire it to my Arduino Uno R3. My final purpose is to connect Arduino to my phone via BT.
I followed the tutorial for the BT modules to hook it up with Arduino, but I can't get past the first example sketches.
when I try the basic sketch, or the passthrough sketch, my code never returns true on bluetooth.available(). So I can't communicate with the bluetooth mate.
I've tried playing with the baudrates, changing Arduino IDE versions and computer settings & OS (Win 7 & Linux). But still no results.
Can anyone guide me towards a solution? Thanks in advance...
This is de sketch I am using:
Code: Select all
https://learn.sparkfun.com/tutorials/us ... mmand-mode/*
Example Bluetooth Serial Passthrough Sketch
by: Jim Lindblom
SparkFun Electronics
date: February 26, 2013
license: Public domain
This example sketch converts an RN-42 bluetooth module to
communicate at 9600 bps (from 115200), and passes any serial
data between Serial Monitor and bluetooth module.
*/
#include <SoftwareSerial.h>
int bluetoothTx = 2; // TX-O pin of bluetooth mate, Arduino D2
int bluetoothRx = 3; // RX-I pin of bluetooth mate, Arduino D3
SoftwareSerial bluetooth(bluetoothTx, bluetoothRx);
void setup()
{
Serial.begin(9600); // Begin the serial monitor at 9600bps
bluetooth.begin(115200); // The Bluetooth Mate defaults to 115200bps
bluetooth.print("$"); // Print three times individually
bluetooth.print("$");
bluetooth.print("$"); // Enter command mode
delay(100); // Short delay, wait for the Mate to send back CMD
bluetooth.println("U,9600,N"); // Temporarily Change the baudrate to 9600, no parity
// 115200 can be too fast at times for NewSoftSerial to relay the data reliably
bluetooth.begin(9600); // Start bluetooth serial at 9600
}
void loop()
{
if(bluetooth.available()) // If the bluetooth sent any characters
{
// Send any characters the bluetooth prints to the serial monitor
Serial.print((char)bluetooth.read());
}
if(Serial.available()) // If stuff was typed in the serial monitor
{
// Send any characters the Serial monitor prints to the bluetooth
bluetooth.print((char)Serial.read());
}
// and loop forever and ever!
}