- Thu Jun 19, 2014 8:16 pm
#172100
Hello Forum members
I have been trying to crack the checksum method for an RC tank controller from Heng Long
the Transmitter and Receiver use a TI CC2500 2.4ghz transceiver module and using a logic analyzer
have got the SPI codes to setup the CC2500 and the stick function data sent from the transmitter to the
tank control receiver board, the codes I have received are
Idle 3F7F82005A AC 120000 CHECKSUM IS AC
Ignition 3F7F82045A B0 120000 CHECKSUM IS B0
Mach Gun 3F7F82025A AE 120000 CHECKSUM IS AE
Main Gun 3F7F82015A AD 120000 CHECKSUM IS AD
BB Gun 3F7F82405A EC 120000 CHECKSUM IS EC
Gun Elevation 3F7F82205A CC 120000 CHECKSUM IS CC
Turret Right 3F7F82085A B4 120000 CHECKSUM IS B4
Turret Left 3F7F82105A BC 120000 CHECKSUM IS BC
Motor Fwd Full 3F0080085A 2D 120000 CHECKSUM IS 2D
Motor Rvs Full 3FFE80085A 2B 120000 CHECKSUM IS 2B
Motor Left Full 3F7F00085A 2A 120000 CHECKSUM IS 2A
Motor Right Full 3F7FFF085A 29 120000 CHECKSUM IS 29
Mach Gun & Gun Elevation together 3F7F83225A CF 120000 CHECKSUM IS CF
Motor Fwd Full & Turrett Right 3F0183085A 37 120000 CHECKSUM IS 37
Motor Fwd Full & Fwd Right Full & Machine Gun 3F0FF3025A B3 120000 CHECKSUM IS B3
Do not know what the 120000 is, it could be the binding code not sure, I would have to look at another
transmitter to see if it changes.
I have tried the simple XOR and summing checksums to no avail and have used reveng thinking it may be
a type of CRC checksum as shown below, as you can see some work providing the correct checksum and others
do not.
would appreciate any help in working out the checksum method for the Heng Long transmitter.
regards Andrew
F:\>reveng -a4 -w8 -s 3F7F82005AAC 3F7F82405AEC
width=8 poly=0x01 init=0x34 refin=false refout=false xorout=0x00 check=0x05 name=(none)
width=8 poly=0x01 init=0xc2 refin=true refout=true xorout=0x00 check=0x72 name=(none)
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82015A
ad correct
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82025A
ae correct
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82045A
a8 wrong should be B0
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82085A
a4 wrong should be B4
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82105A
bc correct
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82205A
8c wrong should be CC
F:\>reveng -c -w 8 -p 01 -i 34 3F0183085A
db wrong should be 37
F:\>reveng -c -w 8 -p 01 -i C2 3F0183085A
2d wrong should be 37
I have been trying to crack the checksum method for an RC tank controller from Heng Long
the Transmitter and Receiver use a TI CC2500 2.4ghz transceiver module and using a logic analyzer
have got the SPI codes to setup the CC2500 and the stick function data sent from the transmitter to the
tank control receiver board, the codes I have received are
Idle 3F7F82005A AC 120000 CHECKSUM IS AC
Ignition 3F7F82045A B0 120000 CHECKSUM IS B0
Mach Gun 3F7F82025A AE 120000 CHECKSUM IS AE
Main Gun 3F7F82015A AD 120000 CHECKSUM IS AD
BB Gun 3F7F82405A EC 120000 CHECKSUM IS EC
Gun Elevation 3F7F82205A CC 120000 CHECKSUM IS CC
Turret Right 3F7F82085A B4 120000 CHECKSUM IS B4
Turret Left 3F7F82105A BC 120000 CHECKSUM IS BC
Motor Fwd Full 3F0080085A 2D 120000 CHECKSUM IS 2D
Motor Rvs Full 3FFE80085A 2B 120000 CHECKSUM IS 2B
Motor Left Full 3F7F00085A 2A 120000 CHECKSUM IS 2A
Motor Right Full 3F7FFF085A 29 120000 CHECKSUM IS 29
Mach Gun & Gun Elevation together 3F7F83225A CF 120000 CHECKSUM IS CF
Motor Fwd Full & Turrett Right 3F0183085A 37 120000 CHECKSUM IS 37
Motor Fwd Full & Fwd Right Full & Machine Gun 3F0FF3025A B3 120000 CHECKSUM IS B3
Do not know what the 120000 is, it could be the binding code not sure, I would have to look at another
transmitter to see if it changes.
I have tried the simple XOR and summing checksums to no avail and have used reveng thinking it may be
a type of CRC checksum as shown below, as you can see some work providing the correct checksum and others
do not.
would appreciate any help in working out the checksum method for the Heng Long transmitter.
regards Andrew
F:\>reveng -a4 -w8 -s 3F7F82005AAC 3F7F82405AEC
width=8 poly=0x01 init=0x34 refin=false refout=false xorout=0x00 check=0x05 name=(none)
width=8 poly=0x01 init=0xc2 refin=true refout=true xorout=0x00 check=0x72 name=(none)
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82015A
ad correct
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82025A
ae correct
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82045A
a8 wrong should be B0
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82085A
a4 wrong should be B4
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82105A
bc correct
F:\>reveng -c -w 8 -p 01 -i 34 3F7F82205A
8c wrong should be CC
F:\>reveng -c -w 8 -p 01 -i 34 3F0183085A
db wrong should be 37
F:\>reveng -c -w 8 -p 01 -i C2 3F0183085A
2d wrong should be 37