- Fri May 16, 2014 12:31 pm
#171200
Sorry if some of these questions may sounds basic.
My understanding of stop masks is that they will prevent anything from convering the pad they are covering, including preventing silk screen or anything, This is important for access to the pads, correct me if I'm wrong.
But why are they required for Vias? A via doesn't need access from the top-level, it just has to connect signals across layers, right.
I'm asking this because I'm getting a warning with Eagle DRC when I have things placed above my Via (via has an automatically added Stop mask), such as another IC.
In this case, I guess if Vias didn't have that stop mask automatically added, I would get no errors. Why are those stop masks auto-added on Vias by Eagle?
Second question, What's the difference between a "Drill" and a "Hole" in Eagle terms? I see the 1x08 adds a Drill component on each pin, do I need to also add a Hole?
Third question, so I'm using the 1x08, and plan to use it with breakaway 0.1" headers. Should the pins be facing one side of the board, while the pads placed on the other side? Or do the pins and the pads go onto the same side?
Thanks in advance,
Joel Fernandes
My understanding of stop masks is that they will prevent anything from convering the pad they are covering, including preventing silk screen or anything, This is important for access to the pads, correct me if I'm wrong.
But why are they required for Vias? A via doesn't need access from the top-level, it just has to connect signals across layers, right.
I'm asking this because I'm getting a warning with Eagle DRC when I have things placed above my Via (via has an automatically added Stop mask), such as another IC.
In this case, I guess if Vias didn't have that stop mask automatically added, I would get no errors. Why are those stop masks auto-added on Vias by Eagle?
Second question, What's the difference between a "Drill" and a "Hole" in Eagle terms? I see the 1x08 adds a Drill component on each pin, do I need to also add a Hole?
Third question, so I'm using the 1x08, and plan to use it with breakaway 0.1" headers. Should the pins be facing one side of the board, while the pads placed on the other side? Or do the pins and the pads go onto the same side?
Thanks in advance,
Joel Fernandes