- Wed Aug 21, 2013 8:05 am
#162839
Hello,
I'm using the Xbee to transmit data from two Flexiforce sensors. I've checked the hardware multiple times and the signals are not interacting. Checking with a multimeter, the input to ADC0 only changes with sensor 1 change and ADC1 only changes with sensor 2 changes. The voltage to the sensors and the ground signal are stable.
However when I parse the Xbee output signal, where 1 is the indicator value of 126, bytes 12 and 13 are controlled by ADC0 but 13 is also affected by the ADC1 input. Byes 14 and 15 are controlled by ADC1 but 15 is also affected by ADC0 input. The attached figures show what my data looks like in Labview and what my DAQ Xbee settings are.
Thank you in advance for any suggestions.
I'm using the Xbee to transmit data from two Flexiforce sensors. I've checked the hardware multiple times and the signals are not interacting. Checking with a multimeter, the input to ADC0 only changes with sensor 1 change and ADC1 only changes with sensor 2 changes. The voltage to the sensors and the ground signal are stable.
However when I parse the Xbee output signal, where 1 is the indicator value of 126, bytes 12 and 13 are controlled by ADC0 but 13 is also affected by the ADC1 input. Byes 14 and 15 are controlled by ADC1 but 15 is also affected by ADC0 input. The attached figures show what my data looks like in Labview and what my DAQ Xbee settings are.
Thank you in advance for any suggestions.
You do not have the required permissions to view the files attached to this post.