- Mon Jul 22, 2013 4:49 am
#161766
I am sending message between two boards (TX and RX). After a message is sent, I put the board in power saving mode, and it is reset after every 1 seconds by watchdog. Later on, I will configure so it send the message every 5 seconds.
The problem is this: without putting in power saving mode, they transmit message very well, and I can see a reset every 1 seconds through LED. If it goes into power saving mode, I can still see it resets (as the LED signals), but no more transmission happens.
By commenting out line 194 as it is now ( or equivalently the 8th to last line), the code works; uncomment it, the transmission does not work anymore, though the chip clearly reset every 1 seconds.
I appreciate any help.
(PS: ignore some random characters, they are comments written in Chinese that can't be displayed here)
The problem is this: without putting in power saving mode, they transmit message very well, and I can see a reset every 1 seconds through LED. If it goes into power saving mode, I can still see it resets (as the LED signals), but no more transmission happens.
By commenting out line 194 as it is now ( or equivalently the 8th to last line), the code works; uncomment it, the transmission does not work anymore, though the chip clearly reset every 1 seconds.
I appreciate any help.
(PS: ignore some random characters, they are comments written in Chinese that can't be displayed here)
Code: Select all
// Ñ¡Ôñ0-30µÄÊý×Ö£¬¼ä¸ôΪ5MHz
#define CHANNEL 8
// µ±µÚÒ»¸ö°ü¹üûÓÐÊÕµ½Ê±£¬ÔÙ·¢Ë͵ĴÎÊý
#define REPEAT 1
// ·¢Ëͼä¸ô:ÃëÊý
#define INTERVAL 1
int channel = CHANNEL * 5;
int interval = INTERVAL * 128;
#include <Nordic\reg24le1.h>
#include <stdint.h>
#include "API.h"
#define PIN32
#ifdef PIN32
sbit S3 = P1^4; // 1/0=δ°´/°´ÏÂ
sbit S2 = P1^3; // 1/0=δ°´/°´ÏÂ
sbit S1 = P1^2; // 1/0=δ°´/°´ÏÂ
sbit LED3 = P0^1; // 1/0=Ãð/ÁÁ
sbit LED2 = P0^2; // 1/0=Ãð/ÁÁ
sbit LED1 = P0^0; // 1/0=Ãð/ÁÁ
#endif
#define INTERRUPT_RFIRQ 9
#define INTERRUPT_TICK 13
#define TX_ADR_WIDTH 5 // RFÊÕ·¢µØÖ·¹²5 bytes
#define TX_PLOAD_WIDTH 20 // Êý¾Ý°ü³¤¶ÈΪ20 bytes
uint8_t const TX_ADDRESS[TX_ADR_WIDTH] = {0x34,0x56,0x78,0x90,0x12}; // ¶¨ÒåRFÊÕ·¢µØÖ·
uint8_t data id_buf[TX_PLOAD_WIDTH]={0xff, 0x01, 0x02, 0x03, 0x04, 0x05};
uint8_t bdata sta;
sbit RX_DR =sta^6;
sbit TX_DS =sta^5;
sbit MAX_RT =sta^4;
uint8_t warn;
/**************************************************
¹¦ÄÜ£ºÑÓʱ
**************************************************/
void delay(uint16_t x)
{
uint16_t i,j;
i=0;
for(i=0;i<x;i++)
{
j=108;
;
while(j--);
}
}
/**************************************************
¹¦ÄÜ£ºÓ²¼þSPI¶Áд
**************************************************/
uint8_t SPI_RW(uint8_t value)
{
SPIRDAT = value;
while(!(SPIRSTAT & 0x02)); // µÈ´ýSPI´«ÊäÍê³É
return SPIRDAT; // ·µ»Ø¶Á³öÖµ
}
/**************************************************
¹¦ÄÜ£ºÐ´RF¼Ä´æÆ÷£¬¶ÁRF״ֵ̬
**************************************************/
uint8_t SPI_RW_Reg(uint8_t reg, uint8_t value)
{
uint8_t status;
RFCSN = 0;
status = SPI_RW(reg); // Ñ¡ÔñRF¼Ä´æÆ÷
SPI_RW(value); // дÈëÊý¾Ý
RFCSN = 1;
return(status); // ·µ»ØRF״ֵ̬
}
/**************************************************
¹¦ÄÜ£º¶ÁRF¼Ä´æÆ÷
**************************************************/
uint8_t SPI_Read(uint8_t reg)
{
uint8_t reg_val;
RFCSN = 0;
SPI_RW(reg); // Ñ¡ÔñRF¼Ä´æÆ÷
reg_val = SPI_RW(0); // ¶Á³öÊý¾Ý
RFCSN = 1;
return(reg_val); // ·µ»ØRF״ֵ̬
}
/**************************************************
¹¦ÄÜ£º°Ñ»º³åÇøµÄ¶à×Ö½ÚÊý¾Ýдµ½RF¼Ä´æÆ÷
**************************************************/
uint8_t SPI_Write_Buf(uint8_t reg, uint8_t *pBuf, uint8_t bytes)
{
uint8_t status,byte_ctr;
RFCSN = 0;
status = SPI_RW(reg); // Ñ¡ÔñRF¼Ä´æÆ÷
for(byte_ctr=0; byte_ctr<bytes; byte_ctr++) // Á¬½ÓдÈëÊý¾Ý
SPI_RW(*pBuf++);
RFCSN = 1;
return(status); // ·µ»ØRF״ֵ̬
}
/**************************************************
¹¦ÄÜ£ºÉèÖÃΪµôµçģʽ
**************************************************/
void PD_Mode(void)
{
RFCE=0;
SPI_RW_Reg(WRITE_REG + CONFIG, 0x0c); // PWR_UP=0
}
/**************************************************
¹¦ÄÜ£ºÉèÖÃΪ·¢Éäģʽ
**************************************************/
void TX_Mode(void)
{
SPI_RW_Reg(WRITE_REG + CONFIG, 0x0e); // Éϵç, CRCΪ2 bytes,½ÓÊÕģʽ,ÔÊÐíRX_DR²úÉúÖжÏ
SPI_Write_Buf(WR_TX_PLOAD, id_buf, TX_PLOAD_WIDTH); // дÊý¾Ýµ½FIFO
RFCE=1; // Æô¶¯·¢Éä
delay(10); // ·¢ÉäÂö³å
RFCE=0;
}
void rf_init(void)
{
RFCE = 0; // RF off
RFCKEN = 1; // RF clock enable
RF = 1; // RF interrupt enable
delay(1000);
SPI_Write_Buf(WRITE_REG + TX_ADDR, TX_ADDRESS, TX_ADR_WIDTH); // setting TX address length
SPI_Write_Buf(WRITE_REG + RX_ADDR_P0, TX_ADDRESS, TX_ADR_WIDTH); // setting RX address length
SPI_RW_Reg(WRITE_REG + EN_AA, 0x01); // automatically respond
SPI_RW_Reg(WRITE_REG + EN_RXADDR, 0x01); // PIPE0 receive package
SPI_RW_Reg(WRITE_REG + SETUP_RETR, 0x11); // retransmit once
SPI_RW_Reg(WRITE_REG + RF_CH, channel); // RF frequency at 2440MHz
SPI_RW_Reg(WRITE_REG + RF_SETUP, 0x20); // -16dBm, 250kbps,
SPI_RW_Reg(WRITE_REG + RX_PW_P0, TX_PLOAD_WIDTH); // PIPE0 received package length
}
void RF_IRQ(void) interrupt INTERRUPT_RFIRQ
{
sta=SPI_Read(STATUS); //read status
SPI_RW_Reg(WRITE_REG+STATUS,0x70); // clear interrupt
}
void main(void)
{
/* watchdog enabled */
CLKLFCTRL=0x01;
WDSV=(interval%256);
delay(10);
WDSV=(interval/256);
/* check for voltage through power-fail comparator*/
/* eanble POF comparator at 2.7V threshold*/
POFCON|=0xE0;
/*check voltage: 0x10: below 2.7V; 0x00: above 2.7V*/
warn = POFCON & 0x10;
/* if voltage above 2.7V, start program */
if(warn==0){
/* ALL interrupts enabled */
EA=1;
EX1=0; // POFIRQ disabled
/*LED control */
P0DIR = 0xf0;
P1DIR = 0xff;
LED2=1; //p0.2
/* RF setting */
rf_init(); // RF initialization
EA=1; // enable ALL interrupts
while(1)
{
TX_Mode(); // send data
while (!(TX_DS|MAX_RT)); // wait transmission end
sta = 0;
PD_Mode(); // turn off RF
LED2=0; //p0.2
//PWRDWN = 0x04; // go into sleep
delay(10);
}
}else{
/* if voltage below 2.7V, go sleep */
PWRDWN=0x04;
}
}