- Sat Jun 01, 2013 6:04 pm
#160086
Using the libraries and examples from https://github.com/sparkfun/WiFly-Shield, I am having issues using the SpiUartTerminal library. I send $$$ to go into command mode, but when sending a command, the output starts out clean but then turns into random data. Here is an example output below. I have WiFly shield revision three.
Code: Select all
Any help is appreciated.CMD
get everything
WiFly Ver 2.32, 02-13-2012 on RN-131
Beacon=100
Probe=5
Reboot=0
OPEN=*OPEN*
CLOEL*EEHO
si6Mca0lhe1ITe
ma$FW
PNP76.:0N5220G712
S.020ROPM=4FSxTO=
AP..D=..1N=v1auau
=898:
liyXmUrv
aPs
iucTo=
Pdx
Dog
n
t=
n
tP
s0f
e,4
io0ahson2Sp=
er
ir1Acn
F=
okx0Ilx
uex
nlxTe=
E=9122
e
ut9
l0
dx
_I
im0
pcx
vIWySPwdFm0
g=
re
A22..55
ta0
n=0eP=
2>