All things pertaining to wireless and RF links

Moderator: phalanx


Postby ahref » Wed Jan 30, 2013 12:22 pm


While i'm aware you are all probably fed up with SM5100B questions I was wandering if you could help me out with the SOCKSTATUS response.

When sending a
Code: Select all

I recieve
Code: Select all

I am keen to debug this myself but am able to post full code if required the question is,

Would anyone know of what the different codes in argument 3 of the response are.

I'm aware that 0104 means not connected yet and that 0102 means connected but what do the others mean?

EDIT: I've been seeing behaviour that seems to demonstrate that 0100 means the connection was not exactly ready. A stray OK occurs after I get the 0100. If this OK occurs before then the code is 0102.

Just got a 2130 in that field.

Seriously If there are 0-9999 codes possible here they must be listed somewhere :'(?
Posts: 1
Joined: Wed Jan 30, 2013 7:54 am

Return to Wireless/RF

Who is online

Users browsing this forum: No registered users and 4 guests