- Fri Dec 21, 2012 7:52 pm
#153426
Hi i have been working on this project for some time now i am using a Ardunino R3 and a honey well HMC6343 digital compass. I did have a post here before but had little help from follow members for over 120 days so i deleted it ,So I hope someone will help now
I would like to add GPS to this set up as the compass is not keeping the Kontiki on course.I am looking at buying the Adafruit Ultimate GPS Breakout .It will be under water as it goes under breaking waves.
So i was wondering if anyone could help me to add a gps to my setup and how i can add it to my code that i have it is a very basic system as when i point the Kontiki in the direction of travel and switch on the Arduino the compass locks onto a bearing and adjusts the servo to keep the craft on its bearing.One other problem i am having is i need to adjust the servo from its center point to allow for propeller torque say 1 to 2 degrees to the right but i am unsure how to add this to my code.I have added my code below
I would like to add GPS to this set up as the compass is not keeping the Kontiki on course.I am looking at buying the Adafruit Ultimate GPS Breakout .It will be under water as it goes under breaking waves.
So i was wondering if anyone could help me to add a gps to my setup and how i can add it to my code that i have it is a very basic system as when i point the Kontiki in the direction of travel and switch on the Arduino the compass locks onto a bearing and adjusts the servo to keep the craft on its bearing.One other problem i am having is i need to adjust the servo from its center point to allow for propeller torque say 1 to 2 degrees to the right but i am unsure how to add this to my code.I have added my code below
Code: Select all
#include <Wire.h>
#include <Serial.h>
#include <Servo.h>
#define compassAddress 0x32 >> 1
#define adjustment 15 //Degress to adjust rudder
#define readDelay 2500 //Time between compass reads
Servo rudder; //Rudder servo object
int rudderAngle = 0; //current angle of the rudder servo
int rudderPosition = 0; //New position for rudder
unsigned int compassHeading = 0;
unsigned int initialHeading = 0;
unsigned int heading = 0;
int offset = 0;
int tempOffset = 0;
int headingShift = 0;
byte compassHeadingBytes[2]; //Heading read bytes from compass
int i = 0;
void setup() {
Serial.begin(115200); //Start the serial port for testing
Wire.begin(); //Start i2c
rudder.attach(9); //Rudder servo on pin 9
while( millis() < 500 ) { //Wait for the compass to initialise
delay(10);
}
rudderAngle = rudder.read(); //Get initial angle of rudder servo
readCompass(); //Get heading from compass
setPosition(); //translate into direction segment
setOffset(); //Set offset to correct heading
adjustPosition(); // Adjust heading to new position
initialHeading = heading; //Save heading as target direction
}
void loop() {
readCompass();
setPosition();
adjustPosition();
setServo();
delay(readDelay);
}
void readCompass() {
//Instruct compass to read echoes
Wire.beginTransmission(compassAddress); // transmit to device
// the address specified in the datasheet is 66 (0x42)
// but i2c adressing uses the high 7 bits so it's 33
Wire.write(0x50); // Send a "Post Heading Data" (0x50) command to the HMC6343
Wire.endTransmission(); // stop transmitting
//Wait for readings
delay(2); // datasheet suggests at least 1 ms
//Request heading reading from compass
Wire.requestFrom(compassAddress, 2); // request 2 bytes from slave device #33
//Receive heading reading from compass
if(2 <= Wire.available()) // if 2 bytes were received
{
for(int i = 0; i<2; i++) {
compassHeadingBytes[i] = Wire.read();
}
}
compassHeading = ((int)compassHeadingBytes[0]<<8) | ((int)compassHeadingBytes[1]); // heading MSB and LSB
compassHeading = compassHeading * 0.1; //Translate heading to degress
}
// Translate Compass reading to directional segment
// LSB = N, MSB = NNE.
void setPosition(){
if ( compassHeading >= 349 || compassHeading <= 11 ) {
heading = 1;
}
else if ( compassHeading >= 12 && compassHeading <= 33 ) {
heading = 2;
}
else if ( compassHeading >= 34 && compassHeading <= 56 ) {
heading = 4;
}
else if ( compassHeading >= 57 && compassHeading <= 78 ) {
heading = 8;
}
else if ( compassHeading >= 79 && compassHeading <= 101 ) {
heading = 16;
}
else if ( compassHeading >= 102 && compassHeading <= 123 ) {
heading = 32;
}
else if ( compassHeading >= 124 && compassHeading <= 146 ) {
heading = 64;
}
else if ( compassHeading >= 147 && compassHeading <= 168 ) {
heading = 128;
}
else if ( compassHeading >= 169 && compassHeading <= 192 ) {
heading = 256;
}
else if ( compassHeading >= 193 && compassHeading <= 213 ) {
heading = 512;
}
else if ( compassHeading >= 214 && compassHeading <= 236 ) {
heading = 1024;
}
else if ( compassHeading >= 237 && compassHeading <= 258 ) {
heading = 2048;
}
else if ( compassHeading >= 259 && compassHeading <= 281 ) {
heading = 4096;
}
else if ( compassHeading >= 282 && compassHeading <= 303 ) {
heading = 8192;
}
else if ( compassHeading >= 304 && compassHeading <= 326 ) {
heading = 16384;
}
else if ( compassHeading >= 327 && compassHeading <= 348 ) {
heading = 32768;
}
}
//Ofset based on segment seting, so initial heading is 256.
void setOffset() {
switch ( heading ) {
case 1:
offset = 1;
break;
case 2:
offset = 2;
break;
case 4:
offset = 3;
break;
case 8:
offset = 4;
break;
case 16:
offset = 5;
break;
case 32:
offset = 6;
break;
case 64:
offset = 7;
break;
case 128:
offset = 8;
break;
case 256:
offset = 9;
break;
case 512:
offset = 10;
break;
case 1024:
offset = 11;
break;
case 2048:
offset = 12;
break;
case 4096:
offset = 13;
break;
case 8192:
offset = 14;
break;
case 16384:
offset = 15;
break;
case 32768:
offset = 16;
break;
}
offset = 8 - offset;
}
// Adjust heading by offset
void adjustPosition(){
unsigned int headingTemp = heading;
if ( offset >= 0 ) {
tempOffset = offset;
while ( tempOffset > 0 ) {
headingShift = headingTemp << 1;
headingTemp = headingShift;
if ( headingTemp == 0 ) {
headingTemp = 1;
}
tempOffset = tempOffset - 1;
}
}
else {
switch (offset) {
case -1:
tempOffset = 1;
break;
case -2:
tempOffset = 2;
break;
case -3:
tempOffset = 3;
break;
case -4:
tempOffset = 4;
break;
case -5:
tempOffset = 5;
break;
case -6:
tempOffset = 6;
break;
case -7:
tempOffset = 7;
break;
case -8:
tempOffset = 8;
break;
}
while ( tempOffset > 0 ) {
headingShift = headingTemp >> 1;
headingTemp = headingShift;
if ( headingTemp == 0 ) {
headingTemp = 32768;
}
tempOffset = tempOffset - 1;
}
}
heading = headingTemp;
}
void setServo() {
unsigned int i,j;
rudderPosition = rudderAngle;
i = heading;
if ( heading < 128 ) {
while ( i < 128){
rudderPosition = rudderPosition - adjustment;
j = i << 1;
i = j;
}
}
if ( heading > 128 ) {
while ( i > 128 ) {
rudderPosition = rudderPosition + adjustment;
j = i >> 1;
i = j;
}
}
rudder.write(rudderPosition);
}
Last edited by boatbandit2 on Fri Dec 21, 2012 9:57 pm, edited 1 time in total.