Austria Micro Systems Lightning Sensor

Have a good idea for a new product for SFE or Olimex? Let us know!

Moderator: phalanx

Re: Austria Micro Systems Lightning Sensor

Postby CircuitBurner » Mon May 27, 2013 9:49 pm

roger that!

A series of rapid events, that can be digested as a modulation form.
Russ Reed - KF5DPO

Wings are for fairies...and runways are for fashion models...
User avatar
CircuitBurner
 
Posts: 116
Joined: Fri Feb 22, 2013 5:05 pm
Location: grand prairie, Texas

Re: Austria Micro Systems Lightning Sensor

Postby SvenGWK » Sun Jun 23, 2013 7:30 am

I have some problems with this sensor.
I have connected it via I²C, address 0x01.
Calibration runs fine with a difference of ~12 Hz to the target frequency of 500 khz.
But the problem is - it is receiving absolutely nothing.
No disturbers, no lightnings so far.
In my opinion, wiring and chip (i use a "selfmade-board") must be ok, because otherwise calibration would fail.
Why it is not providing interrupts?
There must be always "something in the air", right?
I have tested it with my Arduino MEGA and with my Raspberry Pi.
Any clue what i can try now?
SvenGWK
 
Posts: 2
Joined: Sun Jun 23, 2013 7:18 am

Re: Austria Micro Systems Lightning Sensor

Postby fll-freak » Mon Jun 24, 2013 4:38 am

This is similar to my experience with the chip. Although I do get disturbers, I very rarely get strikes for even strong lightning that shakes my windows. Have you adjusted any of the registers? Do you live inside a metal house or one with a metal roof? Have you tried it outside? Have you tried to create a disturber by sparking two AA batteries close to it?
fll-freak
Support Volunteer
 
Posts: 1511
Joined: Tue May 12, 2009 8:23 am
Location: New Hampshire, USA

Re: Austria Micro Systems Lightning Sensor

Postby SvenGWK » Mon Jun 24, 2013 11:27 pm

Hello,
Yes - i think i have tried almost everything possible.
I have generated sparks with the spark source of a lighter.

Now I've switched to SPI communication to try another library for arduino.
Calibration works fine, but this time I have always the "too much noise" interrupt.
Played around with the registers - no chance.
OK, maybe it's right - I have a lot of stuff near the computer, like telephone and WiFi router, but they use much higher frequencies. I will try it outside with my notebook soon.
SvenGWK
 
Posts: 2
Joined: Sun Jun 23, 2013 7:18 am

Re: Austria Micro Systems Lightning Sensor

Postby CircuitBurner » Thu Jun 27, 2013 10:03 pm

the key to an issue like this is possibly in the use of an aerial or wire loop antenna.
I would start trying out variations of these.
Russ Reed - KF5DPO

Wings are for fairies...and runways are for fashion models...
User avatar
CircuitBurner
 
Posts: 116
Joined: Fri Feb 22, 2013 5:05 pm
Location: grand prairie, Texas

Re: Austria Micro Systems Lightning Sensor

Postby fll-freak » Fri Jun 28, 2013 4:11 am

Although a different antenna might have been a better choice, this chip is designed for an LRC antenna with a natural frequency of 500kHz. 500kHz was a good choice as it is an unused part of the spectrum and one where lightning shows up very bright. Changing to a different antenna would not be a possibility.
fll-freak
Support Volunteer
 
Posts: 1511
Joined: Tue May 12, 2009 8:23 am
Location: New Hampshire, USA

Re: Austria Micro Systems Lightning Sensor

Postby SFE-Pearce » Fri Jun 28, 2013 8:54 am

We have a Breakout on the way for this. it's in testing now which, as you can imagine, has been difficult. We should have it ready to go in the next few months.
Pearce
SparkFun Technical Research
User avatar
SFE-Pearce
SFE Guru
 
Posts: 62
Joined: Wed Apr 07, 2010 9:30 am
Location: Colorado

Re: Austria Micro Systems Lightning Sensor

Postby Dave Mueller » Fri Jun 28, 2013 2:31 pm

SFE-Pearce wrote:We have a Breakout on the way for this. it's in testing now which, as you can imagine, has been difficult. We should have it ready to go in the next few months.


Send it to someone in Florida :-)
Or build a spark gap generator.
Dave Mueller
 
Posts: 194
Joined: Sat Apr 30, 2011 8:09 pm

Re: Austria Micro Systems Lightning Sensor

Postby Mee_n_Mac » Fri Jun 28, 2013 5:31 pm

Been plenty'o'lightning this week in fll-freak's neighborhood.
Mee_n_Mac
Support Volunteer
 
Posts: 5628
Joined: Thu Apr 28, 2011 4:10 pm

Re: Austria Micro Systems Lightning Sensor

Postby fll-freak » Sat Jun 29, 2013 5:44 am

Yes there has. Had three storm fronts roll through yesterday. Strikes close enough to rattle one's teeth.

Seriously, if you want a beta tester, I am your man. I have been working on a lightning detector for 3 years now. When the AS3935 came out, I thought my life would get easier, but with the bug on the chip, its been a pain in the but.

Please make sure you can switch between SPI and I2C interfaces and that you can adjust the I2C address. The chip has a bug that makes it difficult to use I2C at the address of 0. You can read my website for more info.
fll-freak
Support Volunteer
 
Posts: 1511
Joined: Tue May 12, 2009 8:23 am
Location: New Hampshire, USA

Re: Austria Micro Systems Lightning Sensor

Postby Lefty4000 » Thu Oct 10, 2013 6:09 am

I also have a setup for this.
If something goes wrong on the sparkfun end, I'll pitch it to them and make sure we have a lightning sensor on here.
Lefty4000
 
Posts: 16
Joined: Sun Jan 15, 2012 7:21 pm

Previous

Return to New Product Ideas

Who is online

Users browsing this forum: No registered users and 0 guests