- Wed Jun 23, 2010 2:05 pm
#103701
Hello,
I've got a problem while configuring Cyclone3 FPGA by SVF-file generated by Quartus.
I'm using Ubuntu 10.4 with OpenOCD 0.4.0, I have established connection with my devboard via JTAG, but SVF loading fails with such a report:
My openocd.cfg file looks like that:
Any suggestions of what's going wrong?
I've got a problem while configuring Cyclone3 FPGA by SVF-file generated by Quartus.
I'm using Ubuntu 10.4 with OpenOCD 0.4.0, I have established connection with my devboard via JTAG, but SVF loading fails with such a report:
Code: Select all
As you can see, OpenOCD correctly identified my chip as EP3C25 (0x020f30dd, according to a datasheet).Open On-Chip Debugger 0.4.0 (2010-06-22-01:22)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.berlios.de/doc/doxygen/bugs.html
1000 kHz
Error: Translation from khz to jtag_speed not implemented
Error: Translation from khz to jtag_speed not implemented
Error: Translation from jtag_speed to khz not implemented
Error: Translation from khz to jtag_speed not implemented
Info : interface specific clock speed value 36515828
Info : JTAG tap: ep3c25f324.tap tap/device found: 0x020f30dd (mfg: 0x06e, part: 0x20f3, ver: 0x0)
Warn : gdb services need one or more targets defined
svf processing file: "led/led.svf"
Error: Translation from khz to jtag_speed not implemented
Command handler execution failed
Error: buffer is not enough, report to author
Error: fail to run command at line 5693
4946 ms used
svf file programmed failed
Command handler execution failed
My openocd.cfg file looks like that:
Code: Select all
My led.svf file is 1.5MB in size.interface usb_blaster
jtag_khz 1000
jtag newtap ep3c25f324 tap -irlen 10 -expected-id 0x020f30dd
init
svf led/led.svf quiet
Any suggestions of what's going wrong?