reading gps data

Your source for all things Atmel.

Moderator: phalanx

Post Reply
galed
Posts: 52
Joined: Fri Sep 25, 2009 4:19 pm
Location: Boulder, CO
Contact:

reading gps data

Post by galed » Fri Dec 25, 2009 12:43 am

I have a gps unit hooked up to USARTD0 on my ATXmega256A3. It came out of the box at 4800 baud, I set it to 9600... I've been able to turn off all but the RMC message and can still query the other ones when i need them. I've been working with the RMC message, but this happens with the others too.

First of all, here's the code:

Code: Select all

void gps_parse()
{
   printf("\nparsing: %s ",gps_string);

   char gps_time [11];
   strcpy(gps_time,"");
   char gps_valid;
   char gps_lattitude [10];
   strcpy(gps_lattitude,"");
   char gps_ns;	  
   char gps_longitude [11];
   strcpy(gps_longitude,"");
   char gps_ew;	 
   char gps_speed [5];
   strcpy(gps_speed,"");
   char gps_heading [7];
   strcpy(gps_heading,"");
   char gps_date [7];
   strcpy(gps_date,"");

   char* token;
   char delim = ',';
   token = strtok(gps_string, &delim);
   if(strcmp(token,"$GPRMC") == 0)
      gps_message_type = RMC;
   else if (strcmp(token,"$GPGLL") == 0)
      gps_message_type = GLL;
   switch(gps_message_type)
   {
      case RMC:

	 strcpy(gps_time, strtok(NULL, &delim));
	 gps_valid = *strtok(NULL, &delim);
	 strcpy(gps_lattitude, strtok(NULL, &delim));
	 gps_ns = *strtok(NULL, &delim);
	 strcpy(gps_longitude, strtok(NULL, &delim));
	 gps_ew = *strtok(NULL, &delim);
	 strcpy(gps_speed, strtok(NULL, &delim));
	 strcpy(gps_heading, strtok(NULL, &delim));
	 strcpy(gps_date, strtok(NULL, &delim));
	 break;
      default:
	 printf("GPS PARSE ERROR\n");
	 break;
   }
	 printf("time: \n%s | ", gps_time);
	 printf("valid: %c | ", gps_valid);
	 printf("lat: %s",gps_lattitude);
	 printf("%c | ", gps_ns);
	 printf("long: %s", gps_longitude);
	 printf("%c | ",gps_ew);
	 printf("speed: %s | ", gps_speed);
	 printf("heading: %s | ", gps_heading);
	 printf("date: %s \n", gps_date);
   strcpy(gps_string,"");
}
gps_string is, well, a string that has a full NMEA message. As the code executes, every time the GPS module sends a new update (1 Hz), what I see in my terminal is something like:

Code: Select all

parsing: $GPRMC,070923.000,A,3851.1384,N,07715.5597,W,0.07,264.53,251209,,*19
time: 
070923.000 | valid: A | lat: 3851.1384N | long: 07715.5597W | speed: 0.07 | heading: 264 | date: 53 
which tells me that it's entered the parsing function, with that $GPRMC string as the input so I can double-check the output.

It seems to be a problem with the strtok() function. You can see that once it gets to the value for the heading (265.53), it treats the period (".") as the delimiter, even though otherwise it's been using a comma

why does it do this? what can I do about it? thanks :)

by the way, gps_string (the full NMEA sentence) is being populated by an ISR:

Code: Select all

ISR(USARTD0_RXC_vect)
{
   char c;
   c = USARTD0.DATA;
   strncat(&gps_string, &c, 1);
   if (c == '\n')
   {
      gps_parse();
   }
}

stevech
Support Volunteer
Posts: 2907
Joined: Sat Jun 05, 2004 8:51 pm
Location: USA, California

Post by stevech » Sat Dec 26, 2009 11:53 pm

rather than having us pore over the code,
Why not start by using one of the many, many C downloads for parsing NMEA?

ISR should not call a library routine such as strncat. Use one of the many available for download UART port drivers with buffered I/O that mates up with stdio.

ISR should not call a main routine like parse which in turn calls other library routines, etc.

ne0x
Posts: 4
Joined: Tue Dec 22, 2009 12:20 pm

Post by ne0x » Sun Dec 27, 2009 7:11 am

Do you have a way to send test strings to this to see what happens with other values for the heading? It might be something other than the presence of the period; it might be its position, it might be the length of the string being tokenized, I'm really not sure.

Of course, you could also try stevech's suggestion, and replace your code with a library call, if that's still going to do what you want in the end.
This is not the signature you're looking for...

stevech
Support Volunteer
Posts: 2907
Joined: Sat Jun 05, 2004 8:51 pm
Location: USA, California

Post by stevech » Sun Dec 27, 2009 12:20 pm

ne0x wrote:Do you have a way to send test strings to this to see what happens with other values for the heading? It might be something other than the presence of the period; it might be its position, it might be the length of the string being tokenized, I'm really not sure.

Of course, you could also try stevech's suggestion, and replace your code with a library call, if that's still going to do what you want in the end.
not strictly a library - as there are many C source code examples of parsing NMEA. I've done C recently for this.

n1ist
Support Volunteer
Posts: 1043
Joined: Wed Mar 22, 2006 11:02 am

Post by n1ist » Sun Dec 27, 2009 7:11 pm

strtok is looking for a null-terminated string for the delimiter, not a single character. Try

Code: Select all

  char delim[] = ",";

By passing in the address of the lone comma, it is taking everything from the comma to the next 0 in memory to be the list of delimeters. I guess one of those bytes is or becomes a period.

/mike

Post Reply