- Wed Jun 17, 2009 6:47 pm
#75217
I bought a bluesmirf silver about a month ago.
This is what I have working with it:
-FTDI usb-serial adapter. Running two terminal programs, one connecting to the USB end and another via bluetooth, I was able to send data between the two terminals. So RX/TX on it is working.
-Arduino Mini - have some sample code that pushes data through the serial. I can connect to it via bluetooth and see the data coming out the other end.
So far so good...
BUT... because its default to 9600, and I need it to run faster (at 115200), I have to go into config mode. And it simply does not work. I've tried to send the "$$$" locally (via the usb-serial adapter), as well as through bluetooth ... but nothing works (no response). The RX/TX on the usb-serial adapter lights up so data is obviously been pushed through the bluetooth connection, but the bluetooth module itself doesn't seem to be responding to the command. I believe the default time limit to get into config mode is within 60 seconds... tried to do it as soon as I can after power up and it still does not work.
Anyone else experience this problem, or have any suggestions?
Thanks in advance,
Johnty
This is what I have working with it:
-FTDI usb-serial adapter. Running two terminal programs, one connecting to the USB end and another via bluetooth, I was able to send data between the two terminals. So RX/TX on it is working.
-Arduino Mini - have some sample code that pushes data through the serial. I can connect to it via bluetooth and see the data coming out the other end.
So far so good...
BUT... because its default to 9600, and I need it to run faster (at 115200), I have to go into config mode. And it simply does not work. I've tried to send the "$$$" locally (via the usb-serial adapter), as well as through bluetooth ... but nothing works (no response). The RX/TX on the usb-serial adapter lights up so data is obviously been pushed through the bluetooth connection, but the bluetooth module itself doesn't seem to be responding to the command. I believe the default time limit to get into config mode is within 60 seconds... tried to do it as soon as I can after power up and it still does not work.
Anyone else experience this problem, or have any suggestions?
Thanks in advance,
Johnty