- Fri Nov 21, 2008 6:13 am
#59582
Hello forum members,
I am using following code to output ACLK, SMCLK and MCLK on corresponding port pins.
void OutputMCLK (void)
{
P5DIR |= 0x10; // Select MCLK as output
P5SEL |= 0x10; // Select system functionality
}
void OutputSMCLK (void)
{
P5DIR |= 0x20; // Select SMCLK as output
P5SEL |= 0x20; // Select system functionality
}
void OutputACLK (void)
{
P5DIR |= 0x40; // Select ACLK as output
P5SEL |= 0x40; // Select system functionality
}
Following is the clock configuration code:
__SelectCrystalOsc proc
BIC #OSCOFF,SR // Turn on osc.
BIS.B #XTS+DIVA_1,BCSCTL1 // HF mode //ACLK Divide by 2
L1 BIC.B #OFIFG,&IFG1 // Clear OFIFG
MOV #0FFh,R15 // Delay
L2 DEC R15
JNZ L2
BIT.B #OFIFG,&IFG1 // Re?test OFIFG
JNZ L1 // Repeat test if needed
BIS.B #SELM1+SELM0,&BCSCTL2 // Select LFXT1CLK
BIS.B #DIVM_3,&BCSCTL2 // Mclk divide by 8 (crystal 1Mhz MCLK=250KHz)
BIS.B #SELS,&BCSCTL2 // Select LFXT1CLK for SMCLK
BIS.B #DIVS_3,&BCSCTL2 // SMClk divide by 8 (crystal 1Mhz SMCLK=250KHz)
ret
endproc
With above code, I am getting proper output at ACLK = 250KHz and MCLK = 1MHz but SMCLK is working at 18 Hz which should be 250KHz. Please clarify the problem in code.
Thanks in advance.
I am using following code to output ACLK, SMCLK and MCLK on corresponding port pins.
void OutputMCLK (void)
{
P5DIR |= 0x10; // Select MCLK as output
P5SEL |= 0x10; // Select system functionality
}
void OutputSMCLK (void)
{
P5DIR |= 0x20; // Select SMCLK as output
P5SEL |= 0x20; // Select system functionality
}
void OutputACLK (void)
{
P5DIR |= 0x40; // Select ACLK as output
P5SEL |= 0x40; // Select system functionality
}
Following is the clock configuration code:
__SelectCrystalOsc proc
BIC #OSCOFF,SR // Turn on osc.
BIS.B #XTS+DIVA_1,BCSCTL1 // HF mode //ACLK Divide by 2
L1 BIC.B #OFIFG,&IFG1 // Clear OFIFG
MOV #0FFh,R15 // Delay
L2 DEC R15
JNZ L2
BIT.B #OFIFG,&IFG1 // Re?test OFIFG
JNZ L1 // Repeat test if needed
BIS.B #SELM1+SELM0,&BCSCTL2 // Select LFXT1CLK
BIS.B #DIVM_3,&BCSCTL2 // Mclk divide by 8 (crystal 1Mhz MCLK=250KHz)
BIS.B #SELS,&BCSCTL2 // Select LFXT1CLK for SMCLK
BIS.B #DIVS_3,&BCSCTL2 // SMClk divide by 8 (crystal 1Mhz SMCLK=250KHz)
ret
endproc
With above code, I am getting proper output at ACLK = 250KHz and MCLK = 1MHz but SMCLK is working at 18 Hz which should be 250KHz. Please clarify the problem in code.
Thanks in advance.