- Thu Aug 28, 2008 11:23 pm
#54535
Hi Guys,
I'm working on a project where I need transmission of data to and from a underwater device to a base station above the water. It is to be used in a pool so unfortunately the water is chlorinated. The device in the water will be worn on a swimmer so it will be very close to the surface vertically, but at times the line of sight transmission will be through a considerable amount of water.
I'm thinking of using some of the relatively low frequency transmitter/reciever sets (315/433 Mhz) so they at least have some sort of ability to get through the water. I have a few questions that someone here might be able to offer some advice on.
1. Do you think I can depend on refraction of the radio signal cutting the transmission length from direct to the signal travelling over the water and then being picked up like it was being tranmitted from a more vertical position.
2. Do you think there is any chance what so ever of any of the 2.4Ghz modules working, particularily the ZigBee modules so i can use mesh networks.
3. What would be a good method of testing connectivity during radio tests? Do you suppose that a simple time count sent from one Arduino to another would suffice (and then just looking where the missing counts are)?
If you would like any additional information, please ask and I'll try and answer to the best of my abilities.
Cheers
Andrew
I'm working on a project where I need transmission of data to and from a underwater device to a base station above the water. It is to be used in a pool so unfortunately the water is chlorinated. The device in the water will be worn on a swimmer so it will be very close to the surface vertically, but at times the line of sight transmission will be through a considerable amount of water.
I'm thinking of using some of the relatively low frequency transmitter/reciever sets (315/433 Mhz) so they at least have some sort of ability to get through the water. I have a few questions that someone here might be able to offer some advice on.
1. Do you think I can depend on refraction of the radio signal cutting the transmission length from direct to the signal travelling over the water and then being picked up like it was being tranmitted from a more vertical position.
2. Do you think there is any chance what so ever of any of the 2.4Ghz modules working, particularily the ZigBee modules so i can use mesh networks.
3. What would be a good method of testing connectivity during radio tests? Do you suppose that a simple time count sent from one Arduino to another would suffice (and then just looking where the missing counts are)?
If you would like any additional information, please ask and I'll try and answer to the best of my abilities.
Cheers
Andrew