Bootloader from Flash

Support for Bloader and Screamer

Moderator: phalanx

Bootloader from Flash

Postby AJ Smith » Tue Jul 29, 2008 8:14 pm

Hi

A buddy of mine is using an LPC2148. He is using USB and is trying since days to implement an USB bootloader but with no success. His bootloader is on the Flash, NOT the RAM. He is using the IAP function to start the bootloader. This seems to work so far. He can delete sectors BUT as soon as he wants to write to the Flash the Flash is unlocked and he can't write to it.

Is the reason maybe that with IAP you can't write to Flash because
it's running from the Flash?

Any ideas why this is not working?
AJ Smith
 
Posts: 1
Joined: Tue Jul 29, 2008 8:02 pm

Postby E-RPMSOFT.COM » Wed Apr 22, 2009 12:30 pm

hmm. formaly this will be working..
---------------------------------------------
E-RPMSOFT.COM
(336) 793-0285
E-RPMSOFT.COM
 
Posts: 2
Joined: Wed Apr 22, 2009 12:28 pm


Return to Boot Loading

Who is online

Users browsing this forum: No registered users and 1 guest