- Tue Apr 13, 2010 4:14 pm
#98470
Dear All,
I am currently facing a problem with programming LPC2478 using ISP.
I m getting the following message everything i try to program LPC2478
Operation Failed. Failed to autobaud - step 1.
I have connected serial port to UART0 of LPC2478
The serial cable connections are as follows:
1-1, 2-3, 3-2, 4-6, 5-5, 6-4, 7-8, 8-7... pin 9 is not connected
While programming the LPC2478, I have put the jumpers ISP_E & RST_E whereas RST_SW1 is kept open
In the Flash Magic,
1. Select Device: LPC2478
COM Port: COM1
Baud Rate: 9600
Interface: None(ISP)
Oscillator(MHz):12
2. Erase all Flash+Code Rd Plot is ticked
3. Hex file is selected
4. Verify after programming
I click on start and then power up the LPC2478 board.
after sometime, the message "Operation Failed. Failed to autobaud - step 1." is popped up.
Can someone help in solving the problem.
I am currently facing a problem with programming LPC2478 using ISP.
I m getting the following message everything i try to program LPC2478
Operation Failed. Failed to autobaud - step 1.
I have connected serial port to UART0 of LPC2478
The serial cable connections are as follows:
1-1, 2-3, 3-2, 4-6, 5-5, 6-4, 7-8, 8-7... pin 9 is not connected
While programming the LPC2478, I have put the jumpers ISP_E & RST_E whereas RST_SW1 is kept open
In the Flash Magic,
1. Select Device: LPC2478
COM Port: COM1
Baud Rate: 9600
Interface: None(ISP)
Oscillator(MHz):12
2. Erase all Flash+Code Rd Plot is ticked
3. Hex file is selected
4. Verify after programming
I click on start and then power up the LPC2478 board.
after sometime, the message "Operation Failed. Failed to autobaud - step 1." is popped up.
Can someone help in solving the problem.
Regards
Sushil...
Sushil...