- Sat Apr 03, 2010 8:57 am
#97702
I am having difficulties getting a WiFly GSX connected to my wireless network which uses DHCP. I have tried using two different LinkSys WRT-54G routers (one the actual access point using security and another running dd-wrt in open mode) and observe similar results. My connections are RX, TX, GND, and a regulated 3.3v supply connected to VDD-BAT & VDD-IN. I have VREG-IN connected to ground.
It seems that I can associate with either access point, but I cannot get DHCP information from either. After the successful association, the GSX reports "DHCP: Start" and that's it. I stay associated, but no IPs are passed to the module. If I assign an IP, gateway, mask, etc. From the GSX standpoint it appears that I'm connected and the module says it is listening on port 2000. However, I am unable to connect to the module or make outgoing connections from the module. That leads me to believe that it really isn't connected.
I have run out of ideas. Has anyone seen this before and found out what the problem is?
Here is some of the output from TerraTerm along with some comments:
It seems that I can associate with either access point, but I cannot get DHCP information from either. After the successful association, the GSX reports "DHCP: Start" and that's it. I stay associated, but no IPs are passed to the module. If I assign an IP, gateway, mask, etc. From the GSX standpoint it appears that I'm connected and the module says it is listening on port 2000. However, I am unable to connect to the module or make outgoing connections from the module. That leads me to believe that it really isn't connected.
I have run out of ideas. Has anyone seen this before and found out what the problem is?
Here is some of the output from TerraTerm along with some comments:
Code: Select all
--after factory RESET and set wlan join 0
get everything
Beacon=100
Probe=5
OPEN=*OPEN*
CLOSE=*CLOS*
REMOTE=*HELLO*
FlushSize=64
MatchChar=0
FlushTimer=10
IdleTimer=0
CmdChar=$
IF=UP
DHCP=ON
IP=0.0.0.0:2000
NM=255.255.255.0
GW=0.0.0.0
HOST=0.0.0.0:2000
PROTO=TCP,
MTU=1460
FLAGS=0x7
BACKUP=0.0.0.0
DNS=0.0.0.0
Name=server1
Backup=backup2
FTP=208.109.78.34:21
File=wifly-GSX.img
User=roving
Pass=Pass123
SSID=roving1
Chan=0
ExtAnt=0
Join=0
Auth=OPEN
Mask=0x1fff
Rate=12, 24 Mb
Linkmon=0
Passphrase=rubygirl
SleepTmr=0
WakeTmr=0
Trigger=0x1
Autoconn=0
IoFunc=0x0
IoMask=0x20f0
PrintLvl=0x1
TimeEna=0
TIMEADR=129.6.15.28:123
Zone=7
Baudrate=9600
Flow=0x0
Mode=0x0
JoinTmr=1000
Replace=0x24
DeviceId=WiFly-GSX
Password=
BCAST=255.255.255.255:55555
Interval=0x7
<2.15>scan
<2.15>
SCAN:Found 1
Num SSID Ch RSSI Sec MAC Address Suites
1 dd-wrt 03 -35 Open 00:14:bf:09:95:e9 104 4
join # 1
Auto-Assoc dd-wrt chan=3 mode=OPEN SCAN OK
Joining dd-wrt now..
<2.15> Associated!
DHCP: Start
(nothing is returned, even after several minutes)
show net
SSid=dd-wrt
Chan=3
Assoc=OK
Rate=12, 24Mb
Auth=OK
Mode=OPEN
DHCP=FAIL
Time=OK
Links=1
<2.15>show connection
8333
Ralph