- Sat Jul 18, 2009 8:53 am
#77255
Is there a cheaper way to directly program a CSR Bluecore chip? The CSR Casira SDK is $3,000.
Where electronics enthusiasts find answers.
In my project , I guess I need to do the following:Answers1: Yes you need to program the Flash memory using the BlueLab.
=============================================
1. Make the Bluecore4 Module as standalone without MCU so have to program the VM app to contain a OPP profiles app.
2. To extract the Firmware from the BlueCore4-Ext FLASH.Answer2: You can extract the firmware from BlueCore4 but it will be in binary format. So how you will work with this data? I think this is wrong approach. You need to use BlueLab and the OEM firmware by CSR. Or at least the preloaded Casira Firmware which exist in BlueLab but I am not sure if it will work properly in pure chip which you will use in your design.
3. To edit and program the extracted Firmware (eg. LM layer)Answer3: Read the Answer2.
4. Reload back the VM app + Modified Firmware to BlueCore4-EXT flash.Answer4: Read the Answer2.
==============================================Answer5: Yes it contain everything from HCI to upper layers and Profiles.
Questions:
=================
- What is really stored inside the BlueCore4-EXT Flash (firmware) ? Does it contain the whole Stack including Link Controller (LC-baseband), Link Manager(LM), HCI or even higher layer like L2CAP/RFCOMM ?
- If Yes, then can we extract it and modify especially the Link Manager (LM) layer code and reload back the whole assembled firmware back to the bluecore4-ext FLASH iC ?Answer6: I dont know maybe you can if you know what to extract and how work with the binary data which you will have.
- I don't know if I can use BlueLab or BlueSuite or need to get some other tools to do the above?Answer7: If you can find the CSR internal development tools then you can do your job. But, as you understand you will need to design your software for that.
- I am not supplied with any firmware from CSR, but the module should have preloaded bluecore4-ext firmware. Where can we get the firmware for BlueCore4-EXT beside from CSR?Answer8: I know only one way: the CSR.
I have to ask you because CSR support won't answer any technical question and won't even allow us to access any CSR app notes,datasheet and reference unless we buy their $3000 Casira kit. How sad is it that we plan to use their IC in our project and that is the "NO-Support" level we got from them.Answers9: And why you think that somebody need to answer to you when you are not their client? But I can tell you that if you will be their client, you will have their support 100% So, just look the reality. Every company have their strategy so you have two choices follow them or not.
Many many many Thanks to you and I really appreciate your help on this.Regards
Hope this help you in some way.
dtd_electronics wrote:Hi electronix79,Probably the digikey has the same product, but it is better ask them not me Send email to digikey for that question.
Is the WML-C46AHR (from BlueRadios sold by digikey) identical to the WML-C46AHR (from Mitsumi). I means this could be used instead to Casira board as you said ?
thanks