- Mon Nov 10, 2008 11:31 am
#58714
Hi, I'd like to attempt a project involving an AVR as the microprocessor, and to add some code to turn it into learning IR remote receiver. It should be noted that i am still relatively new at this kind of thing, and i have almost no programming knowledge at all. I have made a few simple AVR projects, but those were with code that was provided. I have an arduino, and a bunch of Mega8's handy.
basically i want to clone this device:
http://www.tauntek.com/tinyir2-learning ... ceiver.htm
I have some sample AVR based IR recording code, but i don't know that much about programing to modify it to what i need. Ideally it would be nice if someone could help me translate the c code into arduino code.
here are two sample codes that might be useful...
I obtained these codes from here:
http://www.scienceprog.com/ir-remote-co ... ontroller/
http://git.lochraster.org:2080/?p=fd0/rumpus
I also found this arduino code, but it was not very helpful
http://www.arduino.cc/playground/Code/InfraredReceivers
If someone could help me out a little it would be appreciated. I don't expect someone to write all the code for me, nor do i really want that either. I just need a boost to get started.
Thanks,
-Andrew
basically i want to clone this device:
http://www.tauntek.com/tinyir2-learning ... ceiver.htm
I have some sample AVR based IR recording code, but i don't know that much about programing to modify it to what i need. Ideally it would be nice if someone could help me translate the c code into arduino code.
here are two sample codes that might be useful...
Code: Select all
/pin connected to TSOP1736
#define K1 (1<
uint8_t impulse_prev = 0;
uint8_t counter_impulse_1 = 0;
uint8_t flag_rx = 0;
uint8_t counter_impulse_0 = 0;
uint8_t impulse = 0;
uint64_t counter_ik = 0;
uint64_t code = 0;
ISR(TIMER0_OVF_vect)
{
uint8_t c;
uint8_t str[35];
uint64_t i;
//Timer0 initialization
TCNT0=0xFF;
//Invert input signal
if (K1==1) impulse=0; else impulse=1;
if ((impulse_prev==0)&&(impulse==1))
{//rising edge detection
//reset counter
counter_impulse_1=0;
if ((counter_impulse_0>3)&&(flag_rx==1)&&(counter_impulse_0<23))
{//if receiving symbols
if(counter_impulse_0>12)
//logical 1 received
code |=(1<
counter_ik++;
};
};
if((impulse==1)&&(counter_impulse_1<50))
//counting positive pulses
counter_impulse_1++;
if((impulse_prev==1)&&(impulse==0))
{//negative front
counter_impulse_0=0;
if(counter_impulse_1>30)
{//one long synchro pulse
code=0;
counter_ik=0;
flag_rx=1;
}
};
if((impulse==0)&&(flag_rx==1)&(counter_impulse_1<150))
//counting negative pulses
counter_impulse_0++;
if((counter_impulse_0>50)&&(flag_rx==1)&&(impulse==0))
{//end of receive
flag_rx=0;
counter_impulse_0=0;
counter_impulse_1=0;
counter_ik=0;
code=0;
};
impulse_prev=impulse;
}
Code: Select all
#include <avr/io.h>
#include <avr/interrupt.h>
#include "uart.h"
/* constants */
#define MAX 160
/* global variables */
/* allocate 160*2 = 320 byte memory for storing a code,
* this means we can store 80 on/off sequence timings */
volatile uint16_t code[MAX];
/* current index in code[] (default: 0) */
volatile uint8_t pos = 0;
/* current pin state (default: high == idle) */
volatile uint8_t state = 1;
/* signal for the main application that a code has been received
* (default: 0) */
volatile uint8_t done = 0;
/* signal button presses from interrupt to main */
volatile uint8_t button_press;
/* current system mode */
enum {
MODE_OFF = 0,
MODE_DISPLAY = 1,
} mode = MODE_DISPLAY;
/* current viewmode */
enum {
VIEW_VALUE_AND_TIME = 0,
VIEW_VALUE = 1,
VIEW_TIME = 2,
} view = VIEW_VALUE_AND_TIME;
/* call every 10 ms, for buttons at pins PC0-PC3 */
static uint8_t button_sample(void)
{
static uint8_t btn_state = 0b1111; /* initialize state, buttons are active low! */
static uint8_t last_sample = 0b1111; /* initialize old sample */
uint8_t new_sample = PINC & 0b1111; /* read inputs */
/* mark bits which are sampled with the same value */
uint8_t same_sample = (last_sample ^ ~new_sample);
/* all bits set in same_sample now have been sampled with the same value at
* least two times, which means the button has settled */
/* compare the current button state with the most recent sampled value,
* but only for those bits which have stayed the same */
uint8_t state_different = btn_state ^ (new_sample & same_sample);
/* all bits set in state_different have been sampled at least two times
* with the same value, and this value is different from the current button state */
/* if a bit is set in state (means: button is not pressed) AND bit is set
* in state_different (means: input has settled and value is different from state)
* together means: button has been pressed recently */
uint8_t btn_press = btn_state & state_different;
/* toggle all bits for inputs which switched state */
btn_state ^= state_different;
/* store current sample for next time */
last_sample = new_sample;
/* if bit is set in btn_press, a button has been pressed (not released yet) */
return btn_press;
}
/* pin change interrupt 1 service function */
ISR(PCINT1_vect)
{
/* do nothing if we are just processing a code in the main loop,
* or no more space is available for a timer value */
if (done || pos == MAX)
return;
/* if this would be the first timing value ever recorded, and the
* state before was high (=idle), do not record the timing value
* and just reset the timer */
if (state && pos == 0) {
TCNT1 = 0;
/* else record the timing value */
} else {
/* store current timer value in code[]
* and reset the timer */
code[pos++] = TCNT1;
TCNT1 = 0;
}
/* toggle second led */
PORTD ^= _BV(PD3);
/* toggle state */
state = !state;
}
/* timer 1 compare A interrupt service function */
ISR(TIMER1_COMPA_vect)
{
/* do nothing if we are just processing a code in the main loop */
if (done)
return;
/* if some code has been received */
if (pos > 0) {
/* if pos is odd, one last 'off'-timing is missing, fill with zero */
if (pos % 2 == 1)
code[pos++] = 0;
/* signal main */
done = 1;
/* turn on third led */
PORTD |= _BV(PD6);
}
}
/* timer 2 compare A interrupt service function */
ISR(TIMER2_COMPA_vect)
{
/* sample buttons every 10ms */
button_press |= button_sample();
}
int main(void)
{
/* initialize uart */
uart_init();
uart_printf("rumpus ir analyzer\n");
/* configure led pins as outputs and turn leds off */
DDRC |= _BV(PC4);
DDRD |= _BV(PD3) | _BV(PD6) | _BV(PD7);
PORTC &= ~_BV(PC4);
PORTD &= ~(_BV(PD3) | _BV(PD6) | _BV(PD7));
/* configure ir input pin, with pullup */
DDRC &= ~_BV(PC3);
PORTC |= _BV(PC3);
/* configure button input pins, with pullup */
DDRC &= ~(_BV(PC0) | _BV(PC1) | _BV(PC2) | _BV(PC3));
PORTC |= _BV(PC0) | _BV(PC1) | _BV(PC2) | _BV(PC3);
/* wait until pin is high (no ir carrier is detected) */
while(!(PINC & _BV(PC3)));
/* enable pin change interrupt 1 for ir input pin (PC3/PCINT11) */
PCMSK1 |= _BV(PCINT11);
PCICR |= _BV(PCIE1);
/* configure timer1 with prescaler 64 and CTC for measuring ir timings */
TCCR1B = _BV(CS11) | _BV(CS10) | _BV(WGM12);
/* configure timer action after 200ms: 20mhz/64/5 */
OCR1A = F_CPU/5/64;
/* enable OCR1A interrupt */
TIMSK1 = _BV(OCIE1A);
/* configure timer 2 with prescaler 1024 and CTC
* for button sampling */
TCCR2A = _BV(WGM21);
TCCR2B = _BV(CS22) | _BV(CS21) | _BV(CS20);
/* configure compare event a to occur after 10ms and enable interrupt */
OCR2A = F_CPU/1024/100;
TIMSK2 = _BV(OCIE2A);
/* signal user availability by turning on led 1 */
PORTC |= _BV(PC4);
/* enable interrupts */
sei();
/* signal the user that the analyzer part has started by turning led 1 on */
PORTC |= _BV(PC3);
while(1) {
/* if a code has been received */
if (mode == MODE_DISPLAY && done) {
/* print code to serial uart */
uart_printf("complete code received, %u on-off-timings:\n", pos/2);
for (uint8_t i = 0; i < pos; i += 2) {
if (view == VIEW_VALUE_AND_TIME) {
uint32_t on, off;
/* compute timing in microseconds */
on = ((uint32_t)code[i]) * 64 / 20;
off = ((uint32_t)code[i+1]) * 64 / 20;
uart_printf(" %5lu us (%5u) on, %5lu us (%5u) off\n",
on, code[i],
off, code[i+1]);
} else if (view == VIEW_VALUE) {
uart_printf(" %5u on, %5u off\n",
code[i], code[i+1]);
} else if (view == VIEW_TIME) {
uint32_t on, off;
/* compute timing in microseconds */
on = ((uint32_t)code[i]) * 64 / 20;
off = ((uint32_t)code[i+1]) * 64 / 20;
uart_printf(" %5lu us on, %5lu us off\n",
on, off);
}
}
/* turn off second and third led */
PORTD &= ~(_BV(PD3) | _BV(PD6));
/* wait until pin is high (no ir carrier is detected) */
while(!(PINC & _BV(PC3)));
/* reset all global variables */
pos = 0;
state = 1;
done = 0;
}
if (button_press) {
/* first button toggles system mode */
if (button_press & 0b1) {
mode++;
if (mode > MODE_DISPLAY)
mode = MODE_OFF;
if (mode == MODE_OFF) {
uart_printf("ir analyzer switched off\n");
/* disable timer1 and pin change interrupts */
TIMSK1 &= ~_BV(OCIE1A);
PCMSK1 &= ~_BV(PCINT11);
/* turn off led1 */
PORTC &= ~_BV(PC4);
} else if (mode == MODE_DISPLAY) {
uart_printf("scan and display codes\n");
/* clear interrupt flags, enable timer1 and pin change interrupts */
TIFR1 = _BV(OCIE1A);
TIMSK1 |= _BV(OCIE1A);
PCMSK1 |= _BV(PCINT11);
/* turn on led1 */
PORTC |= _BV(PC4);
}
}
/* second button toggles view mode */
if (button_press & 0b10) {
view++;
if (view > VIEW_TIME)
view = VIEW_VALUE_AND_TIME;
if (view == VIEW_VALUE_AND_TIME)
uart_printf("display timer value and time (in us)\n");
else if (view == VIEW_VALUE)
uart_printf("display timer value\n");
else if (view == VIEW_TIME)
uart_printf("display time (in us)\n");
}
button_press = 0;
}
}
}
I obtained these codes from here:
http://www.scienceprog.com/ir-remote-co ... ontroller/
http://git.lochraster.org:2080/?p=fd0/rumpus
I also found this arduino code, but it was not very helpful
http://www.arduino.cc/playground/Code/InfraredReceivers
If someone could help me out a little it would be appreciated. I don't expect someone to write all the code for me, nor do i really want that either. I just need a boost to get started.
Thanks,
-Andrew